Can anyone please give me procedure to flash bin file into KL25Z using command line only?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can anyone please give me procedure to flash bin file into KL25Z using command line only?

606 Views
gaureshvanjare
Contributor I

Can anyone please give me procedure to flash bin file into  KL25Z using command line only?

Labels (1)
0 Kudos
3 Replies

489 Views
BlackNight
NXP Employee
NXP Employee

You could use the GDB commandline for this, see https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/

I hope this helps,

Erich

0 Kudos

489 Views
gaureshvanjare
Contributor I

Thanks for the procedure. Its indeed a great post. Actually I wanted to flash .bin file and not .elf into kl25z using command prompt.

Regards.

0 Kudos

489 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi gauresh,

  What the debugger you are using now?

  If you are using the JLinkGDBServerCL.exe, you can go to the Jlink forum post a question about it, they may more familiar with the bin file downloading with the command line , the Jlink forum link is:

J-Link/Flasher related - SEGGER Forum

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos