Can anyone please give me procedure to flash bin file into KL25Z using command line only?
You could use the GDB commandline for this, see https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/
I hope this helps,
Erich
Hi gauresh,
What the debugger you are using now?
If you are using the JLinkGDBServerCL.exe, you can go to the Jlink forum post a question about it, they may more familiar with the bin file downloading with the command line , the Jlink forum link is:
J-Link/Flasher related - SEGGER Forum
Wish it helps you!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------