Bluetooth SIG Certification of KW36A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth SIG Certification of KW36A

901 Views
ajith_k
Contributor I

Hi,

Is the BLE Stack on KW36A family Bluetooth SIG certified? If yes, please provide the details.

Expecting a quick resolution.

Regards

Labels (1)
0 Kudos
2 Replies

790 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Ajith, I hope you're doing well!

 

KW35A/KW36A and KW35Z/KW36Z are tested and qualified to comply with the Bluetooth 5.0 Core Specification for both Controller and Host designs.

The listings can be found with the following public Declaration IDs: 

  • Kinetis BLE 5.0 Host Declaration ID: D038956
  • Kinetis BLE 5.0 Controller Declaration ID: D038955

 

Please let me know if you need any other information.

 

Best regards,

Sebastian

0 Kudos

790 Views
jay_kanakiya
Contributor I

Hi nxf53124,

Can you share the FCC ID for Host and Controller as well ? 

I am unable to find them on the FCC website

0 Kudos