NAVQ seems mysterious!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NAVQ seems mysterious!

1,897 次查看
kayboku
Contributor I

Up until now I have developed the software I need on my Raspberry pi, using opencv, gstreamer etc. It seems easy to setup and get going, just install rasbian image onto the sd card, put the card in the pi, and off you go!

So my NAVQ arrived yesterday, and I just feel completely lost. There is a preloaded SD card, I can see the master and demo images on there, When the navq computer boots up with a hdmi screen, it goes to a wayland terminal, upon which i can navigate around the SD card. 

I have read and reread the instructions, gitbook, searched youtube for videos, tried a few different things, im just not sure where its at. It seems like the SD is preloaded, yet nothing seems familiar when the navq boots from sd. 

If i can just install ubuntu or something familiar that i can run python etc in, I wil be fine from then on and begin progressing into my drone concepts

0 项奖励
2 回复数

1,869 次查看
iaingalloway
NXP Employee
NXP Employee

1,891 次查看
kayboku
Contributor I

I entered sudo apt update, in the wayland terminal, and the ubuntu appeared a lot in the updates.

SO now I realise that ubuntu (without the GUI) is installed on the sd, so I should be all good to go! 

0 项奖励