LS,
when I want to select an image for an image button or image object, only the preview of the image is shown to select from, but there is no way to check which image it is since the name is not shown
Would it be possible in the next release of GuiGuider to show the name of the image when eg you hoover over the image? Especially with lookalike images (or when experimenting with the same image in a different resolution) it is very hard to know which image is selected
And double-click to select and close the window would be nice too!
Thanks
kind regards,
Rob van Lieshout
PragmaLab
Hi Rob,
Thanks for your suggestion about image name when seleted.
Actually in just released version 1.5.1 we have realized this feature, the effect:
Maybe you can try to import your project into new version of GUI Guider to use this feature.
Hope you have a good experience in V1.5.1.
Best Regards,
Wenbin Yuan
Hello @PragmaLab
Thanks for your sharing, I think this feature is very useful. I have taken request to GUI guider team.
Thanks!
BR
Alice