please show name of the image when selecting one

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

please show name of the image when selecting one

665 次查看
PragmaLab
Contributor II

LS,

when I want to select an image for an image button or image object, only the preview of the image is shown to select from, but there is no way to check which image it is since the name is not shown

PragmaLab_0-1681284904253.png

Would it be possible in the next release of GuiGuider to show the name of the image when eg you hoover over the image? Especially with lookalike images (or when experimenting with the same image in a different resolution) it is very hard to know which image is selected

And double-click to select and close the window would be nice too!

Thanks

kind regards,
Rob van Lieshout
PragmaLab

3 回复数

639 次查看
WenbinYuan
NXP Employee
NXP Employee

Hi Rob,

Thanks for your suggestion about image name when seleted.

Actually in just released version 1.5.1 we have realized this feature, the effect:

image_name_when_selected.png 

Maybe you can try to import your project into new version of GUI Guider to use this feature.

Hope you have a good experience in V1.5.1.

Best Regards,

Wenbin Yuan

0 项奖励

644 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @PragmaLab 

 

This feature will be add in next version V1.6.0, thanks!

 

BR

Alice

0 项奖励

654 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @PragmaLab 

 

Thanks for your sharing, I think this feature is very useful.  I have taken request to GUI guider team.

Thanks!

 

BR

Alice

0 项奖励