deformation of widgets on RT1170 LCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

deformation of widgets on RT1170 LCD

跳至解决方案
1,727 次查看
ZHOU_XIAO
NXP Employee
NXP Employee

Hello all.

I am using the Gui Guider 1.4.0 to create easy sample for RT1170 promotion demo.

The widgets of switch and slides shows well in the simulators (C language)

ZHOU_XIAO_0-1663650053619.png

 

 

However after I write and run the project into target RT1170 with LCD(RK055HDMIPI4M) ,the widgets shows changed and deformation as following pictures

ZHOU_XIAO_1-1663650138797.png

 

By the way I just add these switch and slides widgets by default without any modification.

 

 

Best regards

ZHOU

0 项奖励
回复
1 解答
1,693 次查看
Haibao
NXP Employee
NXP Employee

Hi @ZHOU_XIAO 

There is one workaround for this, you can disable the VGlite under LvConf of IDE setting.

BRs,

Haibao

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,705 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @ZHOU_XIAO ,

I just see this bug is fixed in new version, GUI Guider v1.4.1 RC2. It is in field trial.

 

Regards,

Jing

 

Regards,

Jing

0 项奖励
回复
1,694 次查看
Haibao
NXP Employee
NXP Employee

Hi @ZHOU_XIAO 

There is one workaround for this, you can disable the VGlite under LvConf of IDE setting.

BRs,

Haibao

0 项奖励
回复