variable watch not update in the freemaster 3.2.2.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

variable watch not update in the freemaster 3.2.2.2

2,010 Views
Panasonic_Kevin_Yang
Contributor I

Panasonic_Kevin_Yang_1-1709790342797.pngPanasonic_Kevin_Yang_2-1709790387204.png

Panasonic_Kevin_Yang_0-1709818769090.png

Panasonic_Kevin_Yang_1-1709818827359.pngPanasonic_Kevin_Yang_2-1709818861847.png

 

 

the target hardware is S32K388 and the behavior is same on NXP S32K388 EVB and our own designed HW.

 

The test code on the target is incrementing the test_counter to 100 then back to 0.

I tested with debugger, the code runs OK.

I tried to define the variable as static volatile or just static.  

But the value never change in the freemaster.

And by checking the log, I can see there is error code 0x80000081

please help to provide some ideas what is going wrong.

 

I’m using JLink plugin as the communication method.

 

0 Kudos
17 Replies

1,322 Views
iulian_stan
NXP Employee
NXP Employee

Hi @Panasonic_Kevin_Yang@DouDou1,

We are looking into this issue. In the meantime could you provide some details about the following:

  1. Are you facing this issue when the application is loaded into Flash or Sram, or both ?
  2. Are you running an active debug session at the same time you use FreeMASTER ?
0 Kudos

904 Views
DouDou1
Contributor II

I found that every S32DS program creates a variable called exit_code and decides if it is equal to 0 in the main loop. When I call freemaster, this variable is changed, and the program is finished

0 Kudos

791 Views
Panasonic_Kevin_Yang
Contributor I
our sw won't run into that loop, so it is not the root cause in our case.
0 Kudos

297 Views
DouDou1
Contributor II

You can try to see if the variable has changed, and if it has, then the program will not proceed

0 Kudos

693 Views
iulian_stan
NXP Employee
NXP Employee

Hi,

It seems that JLink performs some default operations on connect. Ex: memory initialization - in this case the behavior you observe may depend on your particular application (what is stored in those regions).

Example logs:

 

SetupTarget() start
Initializing ECC RAM...
  RAMCodeAddr: 0x20000000
  RAMInitAddr: 0x20000010
  RAMInitSize: 0x00007FF0
  InitPattern: 0xDEADBEEF
  ECC RAM initialized successfully
Initializing ECC RAM...
  RAMCodeAddr: 0x20000000
  RAMInitAddr: 0x20400000
  RAMInitSize: 0x00004000
  InitPattern: 0xDEADBEEF
  ECC RAM initialized successfully
SetupTarget() end - Took 25.3ms

 

We are yet to confirm whether it's the root cause. If so, this could possibly be disabled with JLink Scripts as described on JLink's Wiki page.

0 Kudos

685 Views
Panasonic_Kevin_Yang
Contributor I

the behavior remains the same, below is the log showing the script has been ran.

 

03-00000000-00-00000001-01C1: ------J-Link related settings------
J-Link Host interface: USB
J-Link script: **********************************\Example_InitTargetOverride.JLinkScript
J-Link settings file: none
------Target related settings------
Target device: S32K388
Target device parameters: none
Target interface: JTAG
Target interface speed: 4000kHz
Target endian: little

0 Kudos

415 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

what Iulian wrote above is important, the JLink may corrupt a memory by initializing it to the 0xDEADBEEF pattern and causing a HardFault. Using a custom JLinkScript which overrides the SetupTarget might be necessary. 

I was observing slightly similar (but still different) behavior on S32K344. It appears that there might be a DebugEvent escalated to a HardFault when FreeMASTER-JLink connects to the application. Regardless the possible HardFault root cause, let's first make an experiment to confirm that it really occurs.

Please locate your vector table (startup_ARMCM7.c) and implement a two different handlers, one for HardFault and one for DebugMon. Implement each handler as a short endless loop which just increment a global variable (countHardFault, countDebugMon).  Add the two counters to FreeMASTER watch to see if they will count (meaning the theory was correct) or not.

Thanks,
Michal

 

0 Kudos

1,069 Views
pasa_kevin_y
Contributor III

I load the application to flash, never tried to load to ram.

I didn't run debug session while using the freemaster

0 Kudos

1,367 Views
DouDou1
Contributor II

Hi,@Panasonic_Kevin_Yang,

Maybe I have the same problem with you. Have you solved it? If so, can you tell me how it was solved?

0 Kudos

1,706 Views
iulian_stan
NXP Employee
NXP Employee

Hi @Panasonic_Kevin_Yang,

I tried to reproduce your issue, unfortunately, v7.94a was no longer available for download.
I checked latest version (v7.96q), but run into other issues. Eventually, I downgrade to V7.92q and was able to use FreeMASTER with no issue.

Could you check this workaround and let us know if it works for you ?

Kind regards,
Iulian

0 Kudos

1,698 Views
pasa_kevin_y
Contributor III

Thank you for trying on your side,

 

But the behavior remain the same after I re-installed to 7.92q

0 Kudos

1,691 Views
iulian_stan
NXP Employee
NXP Employee

Just to confirm what toolchain you are using - is it NXP's GCC, IAR, DIAB or GHS ?

0 Kudos

1,661 Views
pasa_kevin_y
Contributor III

we are using NXP GCC currently.

0 Kudos

1,999 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

please send a screenshot of your Project Options dialog "Comm" tab (where the plug-in is selected) and send also a screenshot of the JLink plug-in configuration dialog.

Also, please describe your hardware platform (what MCU, board etc.).

Thank you,
Michal

0 Kudos

1,992 Views
Panasonic_Kevin_Yang
Contributor I

Hi Michal,

 

I uploaded to the original post, please help to check it.  Thanks.

0 Kudos

1,974 Views
MichalH
NXP Apps Support
NXP Apps Support

Thank you,

the error code 0x80000081 is not applicable here, this is just an intermediate error returned for old protocol command probed by FreeMASTER for backward compatibility. The overall result is OK (0x0), which means the JLink plug-in "thinks" it is returning a valid data.

We will need to do some experiments to find out what is wrong. I suspect the FreeMASTER reads the correct memory, but the CPU is halted. Is there any other way how you can find out if the application is running (e.g. any LED blinking)? It sometimes happens that during JTAG connect/disconnect process, the core gets reset and/or halted.

Please do these experiments:

  • Make your FreeMASTER variable modifiable and change it from variable watch grid to some other value. Will it work? If my theory is correct, the variable will change, but will remain constant after that.
  • If you use IAR toolchain, please attach the debugger and see if you will be able to pause/resume application execution. FYI: the IAR debugger session shall be able to share the JLink connection with FreeMASTER.
  • If IAR is attached, press the software reset button.

Similar to IAR, you can also use Segger Ozone debugger. This is also able to co-exist with FreeMASTER on the same JLink connection.

I will ask my colleagues to replicate the same HW setup and to try to replicate the issue locally.

Thanks,
Michal

 

0 Kudos

1,971 Views
Panasonic_Kevin_Yang
Contributor I

Hi Michal,

 

Thanks for the advice.

 

I just confirmed, when power-on the MCU and its SW running OK.

Panasonic_Kevin_Yang_0-1709834369254.png

 

the mcu halt when I click on the Go button in freemaster.  do you have any idea why the freemaster halt the mcu execution?

0 Kudos