Unable to find FreeMaster 3.0 on PC

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Unable to find FreeMaster 3.0 on PC

ソリューションへジャンプ
886件の閲覧回数
rparveez
Contributor II

Hi,

I completed the installation process of FreeMaster 3.0 but I was not able to find the application. When I tried to reinstall the application it popped up a message saying already installed and pointed to a folder "NXP FreeMaster". However, that folder did not have correct installation structure neither it had uninstall.exe file (instead had a uninstall.jar file). I deleted the entire folder and tried to install again but still it pops the same abort message (Already Installed and pointing to folder location "NXP FreeMaster") but that folder no longer exist now. 

I need help in reinstalling FreeMaster 3.0 on my PC.

0 件の賞賛
1 解決策
864件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @rparveez,

There are some additional registry entries used by the installer that are located at

C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml

In case this file contains a FreeMASTER entry in <products> list the, back up the file and remove it from the disk. Relaunch the installer.

 

Note: If FreeMASTER is the only product it the mentioned registry file, it is safe to completely remove the file (without backup) as it will be recreated automatically during installation process.

元の投稿で解決策を見る

2 返答(返信)
865件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @rparveez,

There are some additional registry entries used by the installer that are located at

C:\Program Files (x86)\Zero G Registry\.com.zerog.registry.xml

In case this file contains a FreeMASTER entry in <products> list the, back up the file and remove it from the disk. Relaunch the installer.

 

Note: If FreeMASTER is the only product it the mentioned registry file, it is safe to completely remove the file (without backup) as it will be recreated automatically during installation process.

854件の閲覧回数
rparveez
Contributor II

Hi @iulian_stan ,

This solution resolved my issues. Thank you.

 

0 件の賞賛