Can I have a negative input voltage in a comparator pin of MC56F82748?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I have a negative input voltage in a comparator pin of MC56F82748?

跳至解决方案
1,160 次查看
kienfrancis_ure
Contributor II

Hi guys,

I just want to ask if the negative voltage(part of the square waveform) is acceptable to the pin of the comparator inside the DSP (MC56F82748VLH). If yes, is there any effect on having a negative voltage input? Do the comparator would reset through time because of this negative voltage?

Thank you

标记 (1)
1 解答
1,053 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kien,

Pls refer to the following Table 5 in data sheet of MC56F827xx, the analog voltage absolute range is from -0.4V to 4.0V for the ADC analog channel pin and Comparator input pin, if the voltage is out of the range, the chip may be damaged.

The voltage operating range of Comparator input pin is from GND to VDDA.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

在原帖中查看解决方案

1 回复
1,054 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kien,

Pls refer to the following Table 5 in data sheet of MC56F827xx, the analog voltage absolute range is from -0.4V to 4.0V for the ADC analog channel pin and Comparator input pin, if the voltage is out of the range, the chip may be damaged.

The voltage operating range of Comparator input pin is from GND to VDDA.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png