Fast Charger/Adapter (TEA1936+ TEA199x+ TEA1903x/05x); LLC Resonant AC/DC Power (TEA19161+ TEA19162+ TEA1995)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fast Charger/Adapter (TEA1936+ TEA199x+ TEA1903x/05x); LLC Resonant AC/DC Power (TEA19161+ TEA19162+ TEA1995)

Fast Charger/Adapter (TEA1936+ TEA199x+ TEA1903x/05x); LLC Resonant AC/DC Power (TEA19161+ TEA19162+ TEA1995)

NXP provides total USB Type-C AC/DC solutions with higher Power density, security and safety with leading technologies that enables time to market, solving application challenges and complying to key global Power regulations. NXP solution supports USB-PD, BC1.2 and Leader in QC4.0+. Resonant AC/DC supplies have superior efficiency at high power output. The TEA1916+ TEA1995 is a digital controller simplifying the complexity of resonant LLC designs and providing easy tuning. It succeeds the very popular TEA1716 used in many resonant Switch Mode Power Supplies for e.g. PC's & TV's, but the TEA1916 is actually very suitable for any power supply > 75W, e.g. medical, industrial and server power supplies. The TEA1916 uses a new digital cycle-by-cycle architecture (Vcap control) to enable a new type of operation at low-power loads.

附件
100% 有帮助 (1/1)
版本历史
最后更新:
‎09-06-2018 01:57 PM
更新人: