已解决! 转到解答。
Hi FwFan
I have mailed to you with a video.The video will tell you how to debug the code in the stepinto mode.
You must update the firmware with the last version.
You also update you ide with two service pack.
I have got a successful result. The video was from technical support of Freescale.
Hi fish_yu,
I had a problem when I updated my osbdm too. I think you should go back to the older version, things worked okay for me after I went back to the older version. Try the osbdm_cf2_gdi.dll. Don't use the osbdm_jm60_gdi_cfv234.dll. I am not sure this will solve your problems, but it may. You can change this under "Remote Debugging".
Good Luck,
FWFan
Hi Fish_Yu,
Try this file, osbdm_cf2_gdi.dll. You can search for it in your computer. It should be under Program Files/Freescale/... Freescale won't let me attach it because it's not one of the allowable extension. I can email it to you if you have an email address.
Also, try to download the old software on the product website.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5225X&fpsp=1&tab=Design_Tools_Tab
Do you still have the old disk that comes with the demo kit?
FWFan
Hello, I have received your mail. Thank You for your help.
Now ,I have another problem about it. I have ever updated the firmware by using the last firmware which downloaded from freescale Demokit 52259 web.
I copied the osbdm_cf2_gdi.dll into the <CodeWarrior for ColdFire V7.1 installed directory>\bin\Plugins\Support\ColdFire\OSBDM. After done, I modified the configuration of CodeWarrior for ColdFire V7.1, In the IDE,I pressed ALT + F7 to get into a new dialog.In there,I selected INTERNAL_FLASH SETTINGs, And in there, I was continue to press a button named Edit Connection... on the right side. At the same time, A dialog named ColdFire V2-V4 JM60 OSBDM was shown to me.In the current dialog, I pressed Button named Browse , and select the old dll file. and Press all Buttons named OK to close and save current configuration in all dialogs.Now ,I was begin to debug the code. At then, There was a warning dialog to show me. The content of diglog was ColdFire GDI Protocol Adapter : An invalid preference was passed to the coldFire GDI protocol.
On the other words, The GDI Protocol error!
I think the phenomenon was caused by the last Firmware of JM60 that updated by i.
I also consider that i also get failed results if i will never recover the old firmware.
These are my viewpoints.
Cold you tell me how you repair your demokit to debug the Example code?
You updated your firmware?
I have already updated the firmware!How to do the next step?
Hi Fish_Yu,
Let's try the easy way and uninstall your CF 7.1 version.
Shut down your computer afterward and restart.
Make a clean reinstall and only add the CW 7.1.1 patch that
comes with the DVD.
I think this should bring everything back to the normal state.
As for bringing back the sample code to your kit, follow the
M52259DEMOKIT Quick Start Guide. It's the envelope that has
your CW Getting Started DVD. I am sure you can find this guide
on the MCF52259 website.
I reburned the demo kit this way before and it works.
Good Luck,
FWFan
Sorry, I tried,I failed. I,all the while, regard that there are errors between Firmware of JM60 and PC driver of Codewarrior7.1.2. Because i have ever desgined other ele-device based on USB communication for our customer. I am very familiar with USB commnincation, USB driver and Application Program that runs under the Windows Operating System.
I don't know your firmware whether updated successfully. But my firmware really have done successfully.
So, I think that if i can't recover the old firmware , I will never get a normally result,except for get new firmware of JM60 and Service pack for Codewarrior 7.1.2.
I have requested a freescale support service. I think that this is the only way to solve the problem.
Thank You for Your help.
Hi FwFan
I have mailed to you with a video.The video will tell you how to debug the code in the stepinto mode.
You must update the firmware with the last version.
You also update you ide with two service pack.
I have got a successful result. The video was from technical support of Freescale.