09-05-2009
02:21 PM
2,224 次查看

carloscuevas
Contributor III
Hello, I 'm looking forward to use this very nice and cheap DemoKit in a school proyect, but theres something that realy annoys me: I flash the app and run it very nice, I can debug and even I can press reset and close the debugger, the app still runs. But in a power switching (power off and then on) it stops running and I need to run the debugger again and click on "run" to make the app run again. Is there any way to solve this problem? I will really need this board to run standalone. Any help would be very appreciated.
已解决! 转到解答。
1 解答
09-05-2009
11:12 PM
1,358 次查看

carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.
2 回复数
09-05-2009
11:12 PM
1,359 次查看

carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.
09-05-2009
09:29 PM
1,358 次查看

mjbcswitzerland
Specialist V
Hi
Are you sure that you have really flashed the application?
1) Check that the project's target is set for a FLASH version and not RAM version.
2) Ensure that you have used the FLASH tool to program the generated ELF or SREC.
See the following Kirin3 tutorial for step-by-step guide (see chapter 5):
http://www.utasker.com/docs/M5223X/uTaskerV1-4_M5225X.PDF
Regards
Mark
www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."