after install CodeWarrior, "check for update" always have errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

after install CodeWarrior, "check for update" always have errors

1,170 Views
QiujuYe
Contributor III

Hi,

After I install CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe, then use "help -> Check for Updates", always have problems as followings:

cw-error-1.PNG

 

sometimes I repeate "check for updates" a few times, then it will done, but I found no gdb_extensions directory, I want to user serdes confiuration tool, but can not find whole serdes 2 protocol.

cw-error3.PNG

 

PS:My project cycle is very tight, please reply as soon as possible, thank you very much,very thanks.

Best Regards

Qiuju.ye

0 Kudos
3 Replies

1,159 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download CW_ARMv8_v2020.06_b200629GA_Win_Offline from the following link and install it.

https://drive.google.com/file/d/1Kjq1nLYrtIfWAHYrup5Cf-TTEJI9iWiu/view?usp=sharing

Please download com.freescale.armv8.11.5.2.GA.Win.updatesite.210130.zip from the following link, then install it in CodeWarrior IDE from Help->Install New Software->Add->Archive.

https://drive.google.com/file/d/1g4FbibmVuEWQdEhCuaOqMUvs6_xQzzYC/view?usp=sharing

0 Kudos

1,156 Views
QiujuYe
Contributor III

Hi yipingwang,

Thanks for your replay. I install CodeWarrior IDE for another computer, then "check for updates" successfully.   but I have another question,  for LS2088A/LS2084A, serdes 2 are configured two PCIE gen3, the speed is 8G each PCIE, but the serdes2 proctocol ,how to choice, 0x3F or 0x51?  we choice 0x51 for our board before, but In the following picture, I am a little confused.

serdes2-protocol.PNG

 

 

Best  Regards

Qiuju.ye

0 Kudos

1,153 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please create a new thread in https://community.nxp.com/t5/QorIQ/bd-p/qoriq-grl to track your new question.

0 Kudos