Where to change the TSEC3_PHY_ADDR in Linux sources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to change the TSEC3_PHY_ADDR in Linux sources

Jump to solution
636 Views
nagireddychitta
Contributor III

Dear All,

 

I am working on Ls1020ATWR custom platform with a reference board from Freescale as LS1021ATWR.

In my board the TSEC3_PHY_ADDR is modified from 3 to 4. I have changed this in Uboot "ls1021atwr.h" file and see Ethnernet is up and working at UBoot level, but i need to make this change in Linux too to make my network up.

 

I tried going thru dts and dtsi files for this platform, but did not get clue on where to make this change.

If anyone has any idea on this, pls let me know which linux file has this info.

 

Thanks in advance!

 

Best Regards,

Nagi

Labels (1)
0 Kudos
1 Solution
395 Views
lunminliang
NXP Employee
NXP Employee

Hello nagi reddy chitta,

Sorry for late.

Can you please try below in device tree like in ls1021a-twr.dts:

&enet2 {

    phy-handle = <&rgmii_phy1>;

    phy-connection-type = "rgmii-id";

    status = "okay";

};

&mdio0 {      

        ...

    rgmii_phy1: ethernet-phy@1 {

        reg = <0x1>;

    };

      ...

};

Change the tsec3_phy_addr in reg to be "reg = <0x4>".

And the ethernet-phy@ changed to 4, looks like:

rgmii_phy3: ethernet-phy@4 {

                                                reg = <0x4>;

}


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
396 Views
lunminliang
NXP Employee
NXP Employee

Hello nagi reddy chitta,

Sorry for late.

Can you please try below in device tree like in ls1021a-twr.dts:

&enet2 {

    phy-handle = <&rgmii_phy1>;

    phy-connection-type = "rgmii-id";

    status = "okay";

};

&mdio0 {      

        ...

    rgmii_phy1: ethernet-phy@1 {

        reg = <0x1>;

    };

      ...

};

Change the tsec3_phy_addr in reg to be "reg = <0x4>".

And the ethernet-phy@ changed to 4, looks like:

rgmii_phy3: ethernet-phy@4 {

                                                reg = <0x4>;

}


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos