What is the address of L3 cache on P4080ds?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the address of L3 cache on P4080ds?

617 Views
peterzheng
Contributor II

Hi,

 

For P4080ds, the L3 cache (CPC), when it was used as cache instead of SRAM, does it has a fixed memory address?

 

If so, what is the address?

 

Regards,

Peter Zheng

Labels (1)
0 Kudos
3 Replies

359 Views
lunminliang
NXP Employee
NXP Employee

Hi,

I think CPC configuring as L3 Cache doesn't have fixed memory address, why do you need the address?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

359 Views
peterzheng
Contributor II

Hi Lunmin,

Agree with you. The reason I ask this question is I want to run a simple program on one core of P4080. And limit this core to only access 1/8 of L3 cache.

I was thinking if I know the fixed address of L3, then I can write to it directly. But it seems to be impossible now.

So to achieve my purpose, do you have any other approach to make one core only access 1/8 of L3 cache.

Thanks,

Peter

0 Kudos

359 Views
lunminliang
NXP Employee
NXP Employee

Hi,

See the approach I post:

How to partition the L3 Cacahe of P4080 using CodeWarrior?

Regards

Lunmin

0 Kudos