Memory access failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Memory access failed

跳至解决方案
920 次查看
Kavinravi
Contributor II

Hi,

While bringing-up LS1046A-based custom board using CodeWarrior, we encounter “Memory access failed” error.

As shown in the target initialization file, we set the USE_SAFE_RCW = True; But, we got: Memory access fail.

"""
Copyright 2016 Freescale Semiconductor, Inc.
Copyright 2016-2019 NXP.
All Rights Reserved

 This software is owned or controlled by NXP and may only be used strictly in accordance with the
 applicable license terms.  By expressly accepting such terms or by downloading, installing,
 activating and/or otherwise using the software, you are agreeing that you have read, and that you
 agree to comply with and are bound by, such license terms.  If you do not agree to be bound by the
 applicable license terms, then you may not retain, install, activate or otherwise use the software.
"""

import gdb
import time

from cw.dbg import ta
from cw.dbg import flash
from cw.dbg.rcw import HWRcwValidation
from cw.utils import cw_info, cw_warn, cw_error

from initialization import *

# In order to connect to a board with a broken RCW, set the following variable to True
# Override RCW using a safe hard-coded RCW option
USE_SAFE_RCW = True;

#NOR offset value
NOR_CS = 0x0

CORE_CONTEXT = ":ccs:LS1046A:CortexA72#0"
SAP_CORE_CONTEXT = ":ccs:LS1046A:SAP#0"

# Base address for DCFG registers;
# it will be used to test if PBL phase was successful or not
DCFG_BASE_ADDRESS = 0x1EE0000
DCSR_BASE_ADDRESS = 0x20000000

# Target access object
TA = ta.create()

###################################################################
# Prepare environment/convenience variables
###################################################################
def Prepare_Env():
    set_init_params(context=CORE_CONTEXT, dcsr_addr=DCSR_BASE_ADDRESS)
    gdb.execute("set $ddr_addr = 0x80000000")
    gdb.execute("set $ocram_addr = 0x10000000")

###################################################################
# Reset
###################################################################
def Reset():
    if USE_SAFE_RCW:
        # Please make sure SERDES REF CLK is set to 100 MHz (SW4[1:2] = 00)
        # Set rcw_src to the hard-coded RCW option matching the board's DIP SW
        # regarding SYSCLK and differential/single-ended clock source

        # use this when SYSCLK = 66 MHz, single-ended clock source
        # TA.rcw.set_source(0x9A)
        # use this when SYSCLK = 66 MHz, differential clock source
        # TA.rcw.set_source(0x9B)
        # use this when SYSCLK = 100 MHz, single-ended clock source
        # TA.rcw.set_source(0x9E)
        # use this when SYSCLK = 100 MHz, differential clock source
        TA.rcw.set_source(0x9F)

        # add here if you need to override other particular RCW values
        # TA.rcw.set_data({1: 0x40282830, 9: 0x00C12980, 10: 0x00002580})
        TA.rcw.apply()

    else:
        try:
            user_reset = gdb.parse_and_eval("$reset")
            user_reset_delay = int(gdb.parse_and_eval("$reset_delay"))
        except gdb.error:
            user_reset = 1
            user_reset_delay = 0

        if user_reset:
            try:
                gdb.execute("cw_reset %d" % user_reset_delay)
            except gdb.error as exc:
                # check if PBL phase was successful;
                # note 1: target accesses must be executed through SAP core
                # note 2: a PBL error can be detected only when RESET_REQ is set to 'Do nothing'
                TA.set_context(SAP_CORE_CONTEXT)
                HWRcwValidation(TA, DCFG_BASE_ADDRESS).check_for_pbl_error()
                # if check_for_pbl_error does not detect the error, forward the initial exception
                raise exc

    Init_BRR()

    # RCPM_CESRD sticky bit which will get set when you deassert EVT_B0
    # REMOVE EXTERNAL DEBUG REQUEST which we issue in ccs on ccs::reset_to_debug
    CCSR_BE_M(0x20160704, 0x80000000)
    CCSR_BE_M(0x20160708, 0x80000000)
    CCSR_BE_M(0x2016070C, 0x80000000)

    # Safeguard against reset skid on CMSISDAP
    # Clear PC
    TA.reg.write(CORE_CONTEXT, "PC", 0)
    # Clear MMU, caches, aligment checks, WNX in SCTLR_EL3
    SCTLR_EL3 = TA.reg.read(CORE_CONTEXT, "SCTLR_EL3").to_int()
    SCTLR_EL3 = SCTLR_EL3 & 0xFFF7EFF0
    TA.reg.write(CORE_CONTEXT, "SCTLR_EL3", SCTLR_EL3)

###################################################################
# CCI Initialization
###################################################################
def Init_CCI():
    # Set Terminate all barrier transactions bit of CCI-400 Control Register
    # (needed for dsb instruction to succeed when doing coherent reads/writes)
    # It will be disabled after DDR is initialized
    CCSR_LE_M(0x01180000, 0x00000008)

    # Enable snoop requests and DVM messages for A53 cluster slave interface 4
    CCSR_LE_M(0x01185000, 0x00000003)

###################################################################
# Boot Release
###################################################################
def Init_BRR():
    # TODO: when we can detect the current context,
    # release all cores for SMP, current core for AMP

    # First set the secondary cores to debug mode after release
    DCSR_BE_M(0x16002C, 0x0000000E)
    # Write to BRR to release cores
    CCSR_BE_M(0x1EE00E4, 0x0000000F)
    # Clear the halt request for the secondary cores
    DCSR_BE_M(0x16001C, 0x0000000E)

    # Make sure the gdb threads are refreshed just after the BRR initialization
    TA.rc.refresh_threads()

    # Make sure the cores are stopped
    TA.rc.halt()

###################################################################
# DDR Initialization
###################################################################
def A008511_Erratum():
    CCSR_BE_M(0x01080F94, 0x80000000)

def A009803_Erratum():
    DDR_BASE = 0x01080000

    # 1. Configure the DDR registers as normal with parity enabled
    CCSR_BE_M(0x01080114, 0x00401070 | 0x00000020)

    # 2. Set ERR_DISABLE[APED]
    CCSR_BE_M(0x01080E44, 0x00 | 0x00000100)

    # 3. Set DDR_SDRAM_CFG[MEM_EN]
    CCSR_BE_M(0x01080110, 0x45200000 | 0x80000000)

    # 4. Poll for DEBUG_2[30] to be set
    while True:
        time.sleep(0.2)
        debug_2_value = CCSR_BE_D(DDR_BASE + 0xF04)
        if debug_2_value & 0x2 != 0:
            break

    # 5. Clear ERR_DIS[APED]. Parity checking is now enabled
    CCSR_BE_M(0x01080E44, 0x00 & (0xFFFFFFFF ^ 0x00000100))

def A009942_Erratum():
    debug_29_value = CCSR_BE_D(0x01080F70)
    debug_29_value |= 0x0070006F
    CCSR_BE_M(0x01080F70, debug_29_value)

def Init_DDRC():
    '''DDR controller initialization routine'''
    #DDR_SDRAM_CFG
    CCSR_BE_M(0x01080110, 0x45200000)

    #CS0_BNDS
    CCSR_BE_M(0x01080000, 0x7F)

    #CS1_BNDS
    CCSR_BE_M(0x01080008, 0x008000BF)

    #CS2_BNDS
    CCSR_BE_M(0x01080010, 0x00C000FF)

    #CS3_BNDS
    CCSR_BE_M(0x01080018, 0x0100013F)

    #CS0_CONFIG
    CCSR_BE_M(0x01080080, 0x80010312)

    #CS1_CONFIG
    CCSR_BE_M(0x01080084, 0x0202)

    #CS2_CONFIG
    CCSR_BE_M(0x01080088, 0x0202)

    #CS3_CONFIG
    CCSR_BE_M(0x0108008C, 0x0202)

    #CS0_CONFIG_2
    CCSR_BE_M(0x010800C0, 0x00)

    #CS1_CONFIG_2
    CCSR_BE_M(0x010800C4, 0x00)

    #CS2_CONFIG_2
    CCSR_BE_M(0x010800C8, 0x00)

    #CS3_CONFIG_2
    CCSR_BE_M(0x010800CC, 0x00)

    #DDR_SDRAM_CFG_2
    CCSR_BE_M(0x01080114, 0x00401070)

    #DDR_SDRAM_MODE
    CCSR_BE_M(0x01080118, 0x01010211)

    #DDR_SDRAM_MODE_2
    CCSR_BE_M(0x0108011C, 0x00)

    #DDR_SDRAM_MODE_3
    CCSR_BE_M(0x01080200, 0x00)

    #DDR_SDRAM_MODE_4
    CCSR_BE_M(0x01080204, 0x00)

    #DDR_SDRAM_MODE_5
    CCSR_BE_M(0x01080208, 0x00)

    #DDR_SDRAM_MODE_6
    CCSR_BE_M(0x0108020C, 0x00)

    #DDR_SDRAM_MODE_7
    CCSR_BE_M(0x01080210, 0x00)

    #DDR_SDRAM_MODE_8
    CCSR_BE_M(0x01080214, 0x00)

    #DDR_SDRAM_MD_CNTL
    CCSR_BE_M(0x01080120, 0x00000000)

    #DDR_SDRAM_INTERVAL
    CCSR_BE_M(0x01080124, 0x18600618)

    #DDR_DATA_INIT
    CCSR_BE_M(0x01080128, 0xDEADBEEF)

    #DDR_SDRAM_CLK_CNTL
    CCSR_BE_M(0x01080130, 0x02800000)

    #DDR_INIT_ADDR
    CCSR_BE_M(0x01080148, 0x00000000)

    #DDR_INIT_EXT_ADDR
    CCSR_BE_M(0x0108014C, 0x00000000)

    #TIMING_CFG_0
    CCSR_BE_M(0x01080104, 0x8055000C)

    #TIMING_CFG_1
    CCSR_BE_M(0x01080108, 0xBBB48E44)

    #TIMING_CFG_2
    CCSR_BE_M(0x0108010C, 0x0049111C)

    #TIMING_CFG_3
    CCSR_BE_M(0x01080100, 0x010C1000)

    #TIMING_CFG_4
    CCSR_BE_M(0x01080160, 0x00220001)

    #TIMING_CFG_5
    CCSR_BE_M(0x01080164, 0x04401400)

    #DDR_ZQ_CNTL
    CCSR_BE_M(0x01080170, 0x8A090705)

    #DDR_WRLVL_CNTL
    CCSR_BE_M(0x01080174, 0x86750609)

    #DDR_SR_CNTR
    CCSR_BE_M(0x0108017C, 0x00000000)

    #DDR_WRLVL_CNTL_2
    CCSR_BE_M(0x01080190, 0x090A0A0B)

    #DDR_WRLVL_CNTL_3
    CCSR_BE_M(0x01080194, 0x0B0C0C00)

    #DDR_ERR_DISABLE
    CCSR_BE_M(0x01080E44, 0x00)

    #DDR_ERR_INT_EN
    CCSR_BE_M(0x01080E48, 0x00)

    #DDR_ERR_SBE
    CCSR_BE_M(0x01080E58, 0x00010000)

    #DDRCDR_1
    CCSR_BE_M(0x01080B28, 0x80040000)

    #DDRCDR_2
    CCSR_BE_M(0x01080B2C, 0x81)

    #DDR_SDRAM_CFG_3
    CCSR_BE_M(0x01080260, 0x00)

    #TIMING_CFG_7
    CCSR_BE_M(0x0108016C, 0x13340000)

    #TIMING_CFG_8
    CCSR_BE_M(0x01080250, 0x02336800)

    #DQ_MAP0
    CCSR_BE_M(0x01080400, 0x32C57554)

    #DQ_MAP1
    CCSR_BE_M(0x01080404, 0xD4BB0BD4)

    #DQ_MAP2
    CCSR_BE_M(0x01080408, 0x2EC2F554)

    #DQ_MAP3
    CCSR_BE_M(0x0108040C, 0xD8000000)

    #DDR_SDRAM_MODE_9
    CCSR_BE_M(0x01080220, 0x0701)

    #DDR_SDRAM_MODE_10
    CCSR_BE_M(0x01080224, 0x04800000)

    #DDR_SDRAM_MODE_11
    CCSR_BE_M(0x01080228, 0x00)

    #DDR_SDRAM_MODE_12
    CCSR_BE_M(0x0108022C, 0x00)

    #DDR_SDRAM_MODE_13
    CCSR_BE_M(0x01080230, 0x00)

    #DDR_SDRAM_MODE_14
    CCSR_BE_M(0x01080234, 0x00)

    #DDR_SDRAM_MODE_15
    CCSR_BE_M(0x01080238, 0x00)

    #DDR_SDRAM_MODE_16
    CCSR_BE_M(0x0108023C, 0x00)

    #DDR_SDRAM_RCW_3
    CCSR_BE_M(0x010801A0, 0x00)

    #DDR_SDRAM_RCW_4
    CCSR_BE_M(0x010801A4, 0x00)

    #DDR_SDRAM_RCW_5
    CCSR_BE_M(0x010801A8, 0x00)

    #DDR_SDRAM_RCW_6
    CCSR_BE_M(0x010801AC, 0x00)

    A008511_Erratum()

    A009803_Erratum()

    A009942_Erratum()

    #Delay before enable
    time.sleep(0.5)

    #DDR_SDRAM_CFG [MEM_EN] = 1
    #print "Enabling DDR controller"
    CCSR_BE_M(0x01080110, 0xC5200000)

    #wait for DRAM data initialization
    time.sleep(0.5)


###################################################################
# IFC Initialization
###################################################################
def Init_IFC():
    # CSPR_EXT
    CCSR_BE_M(0x0153000C + NOR_CS * 12, 0x00000000)
    # CSPR
    CCSR_BE_M(0x01530010 + NOR_CS * 12, 0x60000101)
    # AMASK
    CCSR_BE_M(0x015300A0 + NOR_CS * 12, 0xF8000000)
    # CSOR
    CCSR_BE_M(0x01530130 + NOR_CS * 12, 0x00008000)

    # IFC_FTIM0
    CCSR_BE_M(0x015301C0 + NOR_CS * 48, 0xC0200410)
    # IFC_FTIM1
    CCSR_BE_M(0x015301C4 + NOR_CS * 48, 0x5000900E)
    # IFC_FTIM2
    CCSR_BE_M(0x015301C8 + NOR_CS * 48, 0x0410501C)
    # IFC_FTIM3
    CCSR_BE_M(0x015301CC + NOR_CS * 48, 0x00000000)
    

###################################################################
# QSPI Initialization
###################################################################
def Init_QSPI():
    # QSPI_CFG
    CCSR_BE_M(0x157015C, 0x20100000)

    # SMPR
    CCSR_BE_M(0x1550108, 0x00000000)

    # QuadSPI_FLSHCR
    CCSR_BE_M(0x155000C, 0x00000303)

    # Set top address for each device
    CCSR_BE_M(0x1550180, 0x44000000)
    CCSR_BE_M(0x1550184, 0x48000000)
    CCSR_BE_M(0x1550188, 0x4C000000)
    CCSR_BE_M(0x155018C, 0x50000000)

    # BUF0CR
    CCSR_BE_M(0x1550010, 0x00000000)
    # BUF3CR
    CCSR_BE_M(0x155001C, 0x80000000)
    # BFGENCR
    CCSR_BE_M(0x1550020, 0x00000000)

    # QuadSPI_MCR
    CCSR_BE_M(0x1550000, 0x000f4000)

###################################################################
# Adds Flash devices for this board
###################################################################
def Config_Flash_Devices():
    fl = flash.create(TA)

    # Add QSPI device
    fl.add_device({"alias": "qspi", "name": "MT25QU01GBBB", "address": 0x40000000, "ws_address": 0x10000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "QSPI"})
    
    # Add eMMC device
    fl.add_device({"alias": "mmc", "name": "SDINBDG4", "address": 0x00000000, "ws_address": 0x80000000, "ws_size": 0x1FFFF, "geometry": "8x1", "controller": "eSDHC"})
   
    #set qspi as current device
    fl.set_current_device("qspi")

###################################################################
# Detect DDR frequency
###################################################################
def Detect_DDR_Freq():
    # Detect DDR data rate from RCWSR1
    SYSCLK = 100

    RCWSR1 = CCSR_BE_D(0x01ee0100)
    MEM_PLL_RAT = (RCWSR1 & 0x3F0000) >> 16

    # DDR freq in MT/s
    DDR_freq = int(MEM_PLL_RAT * SYSCLK)

    return  DDR_freq

###################################################################
# L2 RAM Latency
###################################################################
def Config_L2_RAM_Latency():
    # Initialize the L2 RAM latency
    L2CTLR_EL1 = TA.reg.read(CORE_CONTEXT, "L2CTLR_EL1").to_int()
    # Clear L2 Tag RAM latency and L2 Data RAM latency
    L2CTLR_EL1 &= (~(0x000001C7))
    # Set L2 data ram latency bits [2:0]
    L2CTLR_EL1 |= 0x00000002
    # Set L2 tag ram latency bits [8:6]
    L2CTLR_EL1 |= 0x00000080
    TA.reg.write(CORE_CONTEXT, "L2CTLR_EL1", L2CTLR_EL1)

###################################################################
# This is the actual function called by debugger, flash, etc.
###################################################################
def run_init_file():
    Prepare_Env()

    # Reset with RCW override option (USE_SAFE_RCW)
    Reset()

    Init_CCI()

    #Init_IFC()

    Init_QSPI()

    DDR_freq = Detect_DDR_Freq()
    Init_DDRC(DDR_freq)

    Config_Flash_Devices()

    Config_L2_RAM_Latency()

Kavinravi_0-1707718997471.png

When we set the USE_SAFE_RCW = False:

We got “RCW error encountered. In order to diagnose the error temporarily change the board configuration switches to ignore the assertion of the RESET_REQ_B signal. Please refer to board reference manual in order to locate the appropriate switch that controls this behaviour.

Kavinravi_1-1707719067272.png

 

 

Could someone please help us to resolve the error?

 

Thank you for your support.

Regards,

Kavin

1 解答
895 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The "DDR Initialization" section in CodeWarrior initialization file is only used for LS1046RDB demo board, you need to modify this section according to your custom board.

You could use QCVS DDR tool to assist you to calculate the DDR controller configuration parameters, then do validation and optimization to get the optimized parameters and use them in CW initialization file.

Please refer to https://www.nxp.com.cn/docs/en/user-guide/QCVS_DDR_User_Guide.pdf

 If there is SPD on the target board, please use reading from SPD to create a DDR project. If no, please create a QCVS DDR project with default parameters, then modify Properties panel according to DDR datasheet.

 

在原帖中查看解决方案

3 回复数
587 次查看
Dhanyalakshmi
Contributor III

Hello @Kavinravi 

Were you able to resolve the issue you were facing?

Even i''m facing the same issue.

I hope you reply for this 

Thank You.

0 项奖励
回复
519 次查看
Kavinravi
Contributor II

Hi Dhanyalakshmi,

 

Yes, I modified the board initialization file as per our custom board configuration. This fixed the issue. Please use the DDR validation tool (https://www.nxp.com/docs/en/user-guide/QCVS_DDR_User_Guide.pdf) to generate the code for DDR.

If you have any questions, please create a support ticket with NXP, and they will guide you.

Thank you.

 

0 项奖励
回复
896 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The "DDR Initialization" section in CodeWarrior initialization file is only used for LS1046RDB demo board, you need to modify this section according to your custom board.

You could use QCVS DDR tool to assist you to calculate the DDR controller configuration parameters, then do validation and optimization to get the optimized parameters and use them in CW initialization file.

Please refer to https://www.nxp.com.cn/docs/en/user-guide/QCVS_DDR_User_Guide.pdf

 If there is SPD on the target board, please use reading from SPD to create a DDR project. If no, please create a QCVS DDR project with default parameters, then modify Properties panel according to DDR datasheet.