How to generate .a2l file from codewarrior .map file?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to generate .a2l file from codewarrior .map file?

跳至解决方案
8,698 次查看
hbch
Contributor III
I am using codewarrior for MPC55xx V2.4 and the target is MPC5633m. The .map file generated by the linker can not be converted to .a2l file by Vector ASAP2 Editor which is a tool of CANape. Can anyone help me?
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,271 次查看
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,436 次查看
puliufeng
Contributor I

I met the same problem,how to slove it?  Need help

0 项奖励
回复
4,271 次查看
ronco
NXP Employee
NXP Employee

We haven't used the Vector ASAP2 Editor before but we just installed a demo and the only suggestion we have is to set the  MAP file definition  to Metrowerks.  Take a look at the attached screenshot for an example.  I hope this helps.

 

-Ron

0 项奖励
回复
4,272 次查看
hbch
Contributor III
I am sory to report that the solution does not work at all. The A2l misses variables' names and their addresses. If in standard format, the a2l file can get the variables' names but no addresses. Please refer to the attached file.
Message Edited by hbch on 2009-07-23 12:50 PM
0 项奖励
回复