CW 7.2 fails to start/crashes in Windows 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 7.2 fails to start/crashes in Windows 7

Jump to solution
1,598 Views
FridgeFreezer
Senior Contributor I

Due to the march of technology I've been given an upgraded PC at work, which comes with Windows 7.

 

We are using Codewarrior 7.2 for Coldfire V2/3/4, node-locked using a dongle.

 

I have been through the installation procedure (install CW, HASP, dongle drivers, Flexim), the computer can read the dongle ID in LMtools, and I have the license.dat file from the installation on my old PC (the installation instructions seem to say this is what you should do), but when I start Codewarrior it hangs and I get an error message:

 

Description:  A problem caused this program to stop interacting with Windows.Problem signature:  Problem Event Name: AppHangB1  Application Name: IDE.exe  Application Version: 5.9.0.5293  Application Timestamp: 4af36978  Hang Signature: 6d30  Hang Type: 0  OS Version: 6.1.7601.2.1.0.256.48  Locale ID: 2057  Additional Hang Signature 1: 6d30328803df6e4377768ca04d69ef43  Additional Hang Signature 2: ab04  Additional Hang Signature 3: ab043784006824bfd68330095d0f90a7  Additional Hang Signature 4: 6d30  Additional Hang Signature 5: 6d30328803df6e4377768ca04d69ef43  Additional Hang Signature 6: ab04  Additional Hang Signature 7: ab043784006824bfd68330095d0f90a7

 

Can anyone help?

Labels (1)
0 Kudos
Reply
1 Solution
1,086 Views
FridgeFreezer
Senior Contributor I

Well the answer turned out to be worse than I thought - it wasn't a compatability issue at all, it was the fact that I had chosen not to install Processor Expert, which caused CW to grind to a halt at startup looking for PE, and there was no way to tell it that it's not installed.

 

So, the installer lets you select an option which then breaks the program - nice.

View solution in original post

0 Kudos
Reply
4 Replies
1,086 Views
vier_kuifjes
Senior Contributor I

If I was in your case I would simply reinstall my PC with WinXP, or set up a dual boot system. New PC's come with Win7 installed but that doen't mean one must stick with it...

0 Kudos
Reply
1,086 Views
FridgeFreezer
Senior Contributor I

Marc,

I'm aware of both of those options, my question was an attempt to transport the reader on a dreamlike journey to a whimsical fantasy realm of professional software "just working" on a compatible OS.

 

We have Windows 1.0 on 5.25" floppies in the office cupboard but the blu-ray drive just won't read them :smileysad:

0 Kudos
Reply
1,087 Views
FridgeFreezer
Senior Contributor I

Well the answer turned out to be worse than I thought - it wasn't a compatability issue at all, it was the fact that I had chosen not to install Processor Expert, which caused CW to grind to a halt at startup looking for PE, and there was no way to tell it that it's not installed.

 

So, the installer lets you select an option which then breaks the program - nice.

0 Kudos
Reply
1,086 Views
FridgeFreezer
Senior Contributor I

Just to add I have tried:

- Running in Windows XP compatability mode

- Running as Administrator

- Disabling desktop composition as recommended https://community.freescale.com/message/61562#61562

 

None have made any difference.

0 Kudos
Reply