It was running fine until sometime last week. There is a 1K pullup on the Reset# line. I don't use Watchdog. No stack messing. Stops after a few instructions at a time so it can't be stack overflow.
Unhandled interrupt might be a place, but shouldn't I see it go to the vector or PC=FFFF?
Pod should be OK (guessing) because I can load code and erase, etc.
Thanks.