failled to install "CodeWarrior for MPC5xx v8.7"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failled to install "CodeWarrior for MPC5xx v8.7"

1,553 Views
shuangyu
Contributor I

I failed to install "CodeWarrior for MPC5xx v8.7",tips are as follows:

1.PNG

2.PNG

3 Replies

1,128 Views
EWNakai03
Contributor I

I'm running Windows10 is there newer version I can install.  

0 Kudos

1,137 Views
EWNakai03
Contributor I

I have Codewarrior for MPC5xx v8.7, it can't be installed on Win10 32bit machine.  Do I need a new version of Codewarrior?  If so what version?

Regards,

Errol

0 Kudos

1,444 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

which operating system you use?

CodeWarrior for MPC5xx v8.7 is supported up to Windows XP. If you use some newer Windows operating system, it is not possible to install CodeWarrior into the one.

Regards,

Martin