Can't connect to HCS08 device in Freemaster using PE Micro Multilink FX but non FX Multilinks work fine

取消
显示结果 
搜索替代 
您的意思是: 
已解决

Can't connect to HCS08 device in Freemaster using PE Micro Multilink FX but non FX Multilinks work fine

跳至解决方案
408 次查看
jer
Contributor II

I bought a PE Micro Multilink FX because its supposed to be a bit more robust and we've fried a couple standard ones in our test environment.  I can successfully program and debug parts using the Multilink FX in Codewarrior but can't seem to connect in Freemaster.  The standard Multilink works fine in Freemaster.  

It looks like during the connection wizard when HCS08 is selected for driver it can't find a device using the FX.  If I select any of the other drivers it can find the device just fine.  

I've uninstalled and reinstalled the drivers, both PE and Freemaster, it did not change anything.

Using Freemaster version 2.0.7.0 and Windows 10

标记 (2)
0 项奖励
1 解答
244 次查看
jer
Contributor II

I contacted PE Micro and they sent me a new DLL to replace one in the Freemaster program.  It works fine now.

在原帖中查看解决方案

0 项奖励
1 回复
245 次查看
jer
Contributor II

I contacted PE Micro and they sent me a new DLL to replace one in the Freemaster program.  It works fine now.

0 项奖励