Classic - Is it possible (How) to use HCS12 on Eclipse?

取消
显示结果 
搜索替代 
您的意思是: 

Classic - Is it possible (How) to use HCS12 on Eclipse?

无评分

Classic - Is it possible (How) to use HCS12 on Eclipse?

Classic - How to use HCS12 on Eclipse?

-build and debug a CodeWarrior project-

            Valid for some Classic versions - CW for MCU V6.x, CW for HC12 V5.1, etc ...

 

Configuration used:

                Software

Native installation Win 7 Enterprise 64 bit

                                CodeWarrior HC12 v5.1

                                CodeWarrior for MCU V10.6.4 (Updates 5&6)

                Hardware

                                S12XDT512

                                Multilink Universal rev B

 

 

Introduction

Since 2010 we started to move our development tool chains from Classic IDE to Eclipse.

However we continue to use classic tools for some products as CW for HC12 V5.x for HCs12 devices.

The advantage of HC12 is that all features are used in command line in the IDE.

So we can use another IDE than CodeWarrior IDE as Eclipse for instance.

This doc will show you how to:

  • - Create a new project using CW HC12 build tools chain,
  • - Define the external debugger to debug the HC12 application.

 

Attached you will find:

  • - a zip file including the projects. Recommend to unzip it to c:\temp,
  • - 2 videos explaining Build and Debug processes.

 

More references/information can be found at:

            https://community.freescale.com/message/364157#364157

http://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/

 

NOTE:

For Classic versions using integrated debugger, only the build operation can be done under Eclipse.

When the debugger is not available as standalone version there is no way to define an External Tools in Eclipse.

 

  

Phase 1: Create a Project under Eclipse based on a HC12 project

 

  1. 1-      Create a project for the device you need under HC12 v5.1.

 

  1. 2-      Launch Eclipse and create a new empty project

                File ¦ New ¦ Other …

132666_132666.pngpastedImage_6.png

Enable Show All Wizards and select the C Project (which is otherwise hidden), pressing Next.

132667_132667.pngpastedImage_7.png

Click OK

 

Specify the project name, select an Empty Project under Makefile project with — Other Toolchain — and press Finish:

132668_132668.pngpastedImage_8.png

Now I have an empty project

 

Using Project ¦ Properties specify my Build Command:

                ${system:ECLIPSE_HOME}/../gnu/bin/mingw32-make -j6

  132669_132669.pngpastedImage_9.png
 

  1. 3-      Copy all HC12 V5.1 Sources and config files to Eclipse project

 

  1. 4-      Create a makefile with the menu File ¦ New ¦ Other... ¦ General ¦ File

 

 

Phase 2: Build the project using HC12 build tools chain with makefile

 

  1. 1-      Generate the Commandlines used by HC12 v5.1 to build the project.

By this way you will have the options and other paths used for compiler and linker to build the project.

We can use these information to create the makefile.

132670_132670.pngpastedImage_12.png

132671_132671.pngpastedImage_16.png  

  1. 2-      Create the makefile with the menu menu File ¦ New ¦ Other... ¦ General ¦ File

132672_132672.pngpastedImage_17.png132673_132673.pngpastedImage_18.png

An empty makefile is created.

You need to create your makefile according to your project.

For more details we recommend to refer to the link:

http://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/

 

This is the makefile created for this example.

132674_132674.pngpastedImage_19.png

The makefile created contains 2 operations:

                                all -> build the project and generate Srecord files

                                clean -> remove all generated files

 

  1. 3-      Create 2 make targets

for all and clean operations with the "Make Target" under Window ¦ show View

132675_132675.pngpastedImage_20.png

132676_132676.pngpastedImage_21.png

 

 

Now I can build the project using HC12 v5.1 tools (compiler/Linker) under Eclipse project

 

 

Phase 3: Add External debugger to debug hc12 application

 

HC12 V5.1 is using an external debugger named Hiwave.

This tool is using a config file named .ini.

To use HiWave under Eclipse project, we need to define it as external Debugger.

 

By the Run menu click on External Tools ¦ External Tools Configuration…

132677_132677.pngpastedImage_23.png

Run will launch the Debugger and the project.ini file will be generated in the \Bin folder

                You can edit the ini file and use the info provided in the .ini file of HC12 V5.1 project

 

To use these settings, add the Arguments:

                project.abs -w -Target=icd12 -Prod=project.ini

132678_132678.pngpastedImage_24.png

 

Now the debugger is launched and application loaded on board with Multilink Interface.

标签 (1)
附件
评论

I try to follow the tutorial, but the attached files are not available.

Could you please send me the makefile?

Thanks!

版本历史
修订号:
第1页 共1页
最后更新:
‎01-26-2016 07:41 AM
更新人: