Features
Downloads
Revision History
Known problems and limitations
Workspace cannot contain space in the path
Secure Provisioning Tool does not burn all possible security features that are available. Only those required by the selected boot type are configured.
Mac OS X
Closing application using App Menu "securep | Quit securep" doesn't save the workspace setting. Either save settings using menu "File | Save Settings" or use "File | Exit" or use Close button on title bar, which saves the workpsace settings automatically.
Selection of wrong UART in connection dialog may cause the test connection operation takes too long and hang up. Killing sdphost and blhost processes will shorten the dialog freeze.
Windows
Workspace cannot be placed on different disk drive letter then the application is installed.
i.MX RT10xx
BT_FUSE_SEL is not burned so the boot device is based on corresponding GPIO pins.
Parameter "enable_encrypted_XIP" in write script is not properly supported and might not work; this feature is not used in GUI.
LPC Signed Boot Type:
Write requires keys selected on Build tab
Confirmation dialog for enabling security is displayed even security is already enabled
Write scripts requires the cmpa.bin and cfpa.bin files exist on the disk; on CLI it is necessary to manually modify write script to create them
LPC Trust Zone
CLI does not allow to set/override the Trust Zone Settings. If Trust Zone has to be configured and applied in CLI,
workspace has to be configured with Trust Zone settings in GUI in advance.Configuration of Trust Zone is not supported for Unsigned image
ここにコメントを追加するには、ご登録いただく必要があります。 ご登録済みの場合は、ログインしてください。 ご登録がまだの場合は、ご登録後にログインしてください。