Hi,
There is a strange question,when i program MC9S08AW60 CFUE.
I program a mass of MC9S08AW60 CFUE chip with USBDM.but only one chip has the question as follow.
I have two programs .program2 can be programed with no error.But program1 meet the question.
program2 is larger than program1.
So i'm confused.
Hello,
If this is occurring for a single device only, maybe this device is faulty. I would assume that attempting to program an improperly erased device may cause this error.
Regards,
Mac
Hello,
I find the reason .I chose chip type as MC9S08AW32 when i new a project. so to program some chips is ok and to program some chips is error.when i set chip type as MC9S08AW60,it's ok.
Hi Baode,
I haven't ever used USBBDM, I recommend you to raise this question to USBBDM's vendor.
If you use PE USBMultilink, I may provide some help. Hope you understand.