fl::target -lc "Test_Cw-core00_RAM_T2080_Download" fl::target -b 0x2000 0x30000 fl::target -v off -l off cmdwin::fl::device -d "MT29F4G08ABBDA-IFC" -o "512Mx8x1" -a 0x0 0x1fffffff cmdwin::fl::image -f "D:\\nandboot\\u-boot-with-spl-pbl.bin" -t "Auto Detect" -re on -r 0x0 0x1fffffff -oe on -o 0x0 cmdwin::fl::erase image Beginning Operation ... ------------------------- Auto-detection is successful. File is of type Binary/Raw Format. Performing target initialization ... Downloading Flash Device Driver ... Reading flash ID ... Erasing Sector 0x00000000 to 0x0001FFFF Erasing Sector 0x00020000 to 0x0003FFFF Erasing Sector 0x00040000 to 0x0005FFFF Erasing Sector 0x00060000 to 0x0007FFFF Erasing Sector 0x00080000 to 0x0009FFFF Erasing Sector 0x000A0000 to 0x000BFFFF Erasing Sector 0x000C0000 to 0x000DFFFF Erasing ... Erase Command Succeeded cmdwin::fl::write Beginning Operation ... ------------------------- Using restricted address range 0x00000000 to 0x1FFFFFFF Programming file D:\nandboot\u-boot-with-spl-pbl.bin Auto-detection is successful. File is of type Binary/Raw Format. Downloading Flash Device Driver ... Reading flash ID ... Auto-detection is successful. File is of type Binary/Raw Format. Downloading 0x00010000 bytes to be programmed at 0x00000000 Downloading 0x00010000 bytes to be programmed at 0x00010000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x00020000 Downloading 0x00010000 bytes to be programmed at 0x00030000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x00040000 Downloading 0x00010000 bytes to be programmed at 0x00050000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x00060000 Downloading 0x00010000 bytes to be programmed at 0x00070000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x00080000 Downloading 0x00010000 bytes to be programmed at 0x00090000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x000A0000 Downloading 0x00010000 bytes to be programmed at 0x000B0000 Executing program .... Program Command Succeeded Downloading 0x00010000 bytes to be programmed at 0x000C0000 Downloading 0x00005B78 bytes to be programmed at 0x000D0000 Executing program .... Program Command Succeeded