U-Boot SPL 2022.04 (Oct 09 2022 - 00:33:13 +0800) Can't find PMIC:PFUZE100 DDRINFO: start DRAM init DDRINFO: DRAM rate 3200MTS DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot Trying to boot from MMC1 Booting from bootloader_a... U-Boot 2022.04 (Oct 09 2022 - 00:33:13 +0800) CPU: i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz) CPU: Commercial temperature grade (0C to 95C) at 33C Reset cause: POR Model: NXP i.MX8MQ EVK DRAM: 3 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50] Core: 76 devices, 24 uclasses, devicetree: separate MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment [*]-Video Link 0 (1280 x 720) [0] display-controller@32e00000, video [1] hdmi@32c00000, display In: serial Out: serial Err: serial BuildInfo: - ATF 9202efc flash target is MMC:0 Net: Could not get PHY for FEC0: addr 0 Could not get PHY for FEC0: addr 0 No ethernet found. Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 In boota get fastboot lock status error. Set lock status Verifying slot _a ... verify OK, boot 'boot_a' Kernel load addr 0x40480000 size 48651 KiB kernel @ 40480000 (50462720) ramdisk @ 44680000 (19111951) fdt @ 43620400 (50657) Moving Image from 0x40480000 to 0x40600000, end=43620000 ## Flattened Device Tree blob at 43620400 Booting using the fdt blob at 0x43620400 Using Device Tree in place at 0000000043620400, end 000000004362f9e0 Starting kernel ... [ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000][ T0] Linux version 5.15.41-android13-8-00055-g4f5025129fe8-ab8949913 (build-user@build-host) (Android (8508608, based on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #1 SMP PREEMPT Mon Aug 15 18:33:14 UTC 2022 [ 0.000000][ T0] Machine model: NXP i.MX8MQ EVK [ 0.000000][ T0] Stack Depot is disabled [ 0.000000][ T0] efi: UEFI not found. [ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x00000000f8000000, size 40 MiB [ 0.000000][ T0] OF: reserved mem: initialized node secure_mm@f8000000, compatible id shared-dma-pool [ 0.000000][ T0] kvm [0]: Reserved 22 MiB at 0xfe200000 [ 0.000000][ T0] Zone ranges: [ 0.000000][ T0] DMA32 [mem 0x0000000040000000-0x00000000ffffffff] [ 0.000000][ T0] Normal empty [ 0.000000][ T0] Movable zone start for each node [ 0.000000][ T0] Early memory node ranges [ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000f7ffffff] [ 0.000000][ T0] node 0: [mem 0x00000000f8000000-0x00000000fa7fffff] [ 0.000000][ T0] node 0: [mem 0x00000000fa800000-0x00000000ffffffff] [ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x00000000ffffffff] [ 0.000000][ T0] cma: Reserved 1280 MiB at 0x0000000090000000 [ 0.000000][ T0] psci: probing for conduit method from DT. [ 0.000000][ T0] psci: PSCIv1.1 detected in firmware. [ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs [ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000][ T0] psci: SMC Calling Convention v1.2 [ 0.000000][ T0] Load bootconfig: 1063 bytes 67 nodes [ 0.000000][ T0] percpu: Embedded 29 pages/cpu s81472 r8192 d29120 u118784 [ 0.000000][ T0] Detected VIPT I-cache on CPU0 [ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0 [ 0.000000][ T0] CPU features: detected: GIC system register CPU interface [ 0.000000][ T0] CPU features: detected: ARM erratum 845719 [ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 774144 [ 0.000000][ T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 init=/init firmware_class.path=/vendor/firmware loop.max_part=7 bootconfig transparent_hugepage=never cma=1280M moal.mod_para=wifi_mod_para.conf pci=nomsi cpuidle.off=1 bootconfig buildvariant=userdebug [ 0.000000][ T0] cgroup: Disabling pressure control group feature [ 0.000000][ T0] Unknown kernel command line parameters "buildvariant=userdebug", will be passed to user space. [ 0.000000][ T0] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000][ T0] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off [ 0.000000][ T0] Memory: 1247676K/3145728K available (26816K kernel code, 2378K rwdata, 16812K rodata, 2496K init, 591K bss, 587332K reserved, 1310720K cma-reserved) [ 0.000000][ T0] random: get_random_u64 called from kmem_cache_open+0x2c/0x38c with crng_init=0 [ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000][ T0] trace event string verifier disabled [ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation. [ 0.000000][ T0] rcu: RCU event tracing is enabled. [ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled. [ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4. [ 0.000000][ T0] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000][ T0] Trampoline variant of Tasks RCU enabled. [ 0.000000][ T0] Tracing variant of Tasks RCU enabled. [ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000][ T0] GICv3: 128 SPIs implemented [ 0.000000][ T0] GICv3: 0 Extended SPIs implemented [ 0.000000][ T0] GICv3: Distributor has no Range Selector support [ 0.000000][ T0] Root IRQ handler: gic_handle_irq.32972.cfi_jt [ 0.000000][ T0] GICv3: 16 PPIs implemented [ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000 [ 0.000000][ T0] ITS: No ITS available, not enabling LPIs [ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none). [ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____) [ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.33MHz (phys). [ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns [ 0.000000][ T0] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns [ 0.000593][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333) [ 0.000613][ T0] pid_max: default: 32768 minimum: 301 [ 0.000766][ T0] LSM: Security Framework initializing [ 0.000822][ T0] SELinux: Initializing. [ 0.001002][ T0] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.001032][ T0] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.003342][ T1] rcu: Hierarchical SRCU implementation. [ 0.004355][ T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build [ 0.004600][ T1] EFI services will not be available. [ 0.004996][ T1] smp: Bringing up secondary CPUs ... [ 0.005740][ T0] Detected VIPT I-cache on CPU1 [ 0.005773][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000 [ 0.005816][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.006595][ T0] Detected VIPT I-cache on CPU2 [ 0.006616][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000 [ 0.006640][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 0.007381][ T0] Detected VIPT I-cache on CPU3 [ 0.007400][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000 [ 0.007422][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 0.007513][ T1] smp: Brought up 1 node, 4 CPUs [ 0.007557][ T1] SMP: Total of 4 processors activated. [ 0.007565][ T1] CPU features: detected: 32-bit EL0 Support [ 0.007572][ T1] CPU features: detected: 32-bit EL1 Support [ 0.007580][ T1] CPU features: detected: CRC32 instructions [ 0.007591][ T1] CPU features: detected: Protected KVM [ 0.007712][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching [ 0.039578][ T1] CPU: All CPU(s) started at EL2 [ 0.039633][ T18] alternatives: patching kernel code [ 0.053857][ T1] Registered cp15_barrier emulation handler [ 0.053891][ T1] Registered setend emulation handler [ 0.053906][ T1] KASLR disabled due to lack of seed [ 0.054082][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.054121][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear) [ 0.099477][ T1] pinctrl core: initialized pinctrl subsystem [ 0.100705][ T1] NET: Registered PF_NETLINK/PF_ROUTE protocol family [ 0.103436][ T1] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.103780][ T1] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.103842][ T1] audit: initializing netlink subsys (disabled) [ 0.104040][ T43] audit: type=2000 audit(0.100:1): state=initialized audit_enabled=0 res=1 [ 0.104595][ T1] thermal_sys: Registered thermal governor 'step_wise' [ 0.104601][ T1] thermal_sys: Registered thermal governor 'user_space' [ 0.104610][ T1] thermal_sys: Registered thermal governor 'power_allocator' [ 0.105108][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.105225][ T1] ASID allocator initialised with 65536 entries [ 0.105357][ T1] Serial: AMBA PL011 UART driver [ 0.123675][ T1] platform 30a90000.csi1_bridge: Fixing up cyclic dependency with 30a70000.mipi_csi1 [ 0.125299][ T1] platform 30b80000.csi2_bridge: Fixing up cyclic dependency with 30b60000.mipi_csi2 [ 0.127801][ T1] platform 32e00000.display-controller: Fixing up cyclic dependency with 32c00000.hdmi [ 0.145209][ T48] cryptomgr_test (48) used greatest stack depth: 14384 bytes left [ 0.151530][ T1] iommu: Default domain type: Translated [ 0.151559][ T1] iommu: DMA domain TLB invalidation policy: strict mode [ 0.152196][ T1] SCSI subsystem initialized [ 0.152405][ T1] usbcore: registered new interface driver usbfs [ 0.152450][ T1] usbcore: registered new interface driver hub [ 0.152494][ T1] usbcore: registered new device driver usb [ 0.152658][ T1] mc: Linux media interface: v0.10 [ 0.152691][ T1] videodev: Linux video capture interface: v2.00 [ 0.152794][ T1] pps_core: LinuxPPS API ver. 1 registered [ 0.152804][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.152825][ T1] PTP clock support registered [ 0.152861][ T1] EDAC MC: Ver: 3.0.0 [ 0.153762][ T1] Advanced Linux Sound Architecture Driver Initialized. [ 0.154288][ T1] Bluetooth: Core ver 2.22 [ 0.154322][ T1] NET: Registered PF_BLUETOOTH protocol family [ 0.154331][ T1] Bluetooth: HCI device and connection manager initialized [ 0.154347][ T1] Bluetooth: HCI socket layer initialized [ 0.154358][ T1] Bluetooth: L2CAP socket layer initialized [ 0.154399][ T1] Bluetooth: SCO socket layer initialized [ 0.154595][ T1] nfc: nfc_init: NFC Core ver 0.1 [ 0.154643][ T1] NET: Registered PF_NFC protocol family [ 0.155214][ T1] clocksource: Switched to clocksource arch_sys_counter [ 0.206358][ T1] VFS: Disk quotas dquot_6.6.0 [ 0.206441][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.207533][ T1] NET: Registered PF_INET protocol family [ 0.207740][ T1] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.209821][ T1] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear) [ 0.210063][ T1] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.210458][ T1] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear) [ 0.211014][ T1] TCP: Hash tables configured (established 32768 bind 32768) [ 0.211147][ T1] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.211288][ T1] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear) [ 0.211493][ T1] NET: Registered PF_UNIX/PF_LOCAL protocol family [ 0.211536][ T1] NET: Registered PF_XDP protocol family [ 0.211554][ T1] PCI: CLS 0 bytes, default 64 [ 0.212131][ T9] Trying to unpack rootfs image as initramfs... [ 0.215715][ T1] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.216518][ T1] kvm [1]: IPA Size Limit: 40 bits [ 0.241419][ T1] kvm [1]: disabling GICv2 emulation [ 0.241478][ T1] kvm [1]: GIC system register CPU interface enabled [ 0.241700][ T1] kvm [1]: vgic interrupt IRQ9 [ 0.241957][ T1] kvm [1]: Protected nVHE mode initialized successfully [ 0.246849][ T1] Initialise system trusted keyrings [ 0.247174][ T1] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 0.256332][ T1] fuse: init (API version 7.34) [ 0.304011][ T1] Key type asymmetric registered [ 0.304056][ T1] Asymmetric key parser 'x509' registered [ 0.304309][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 239) [ 0.304356][ T1] io scheduler mq-deadline registered [ 0.304368][ T1] io scheduler kyber registered [ 0.304525][ T1] io scheduler bfq registered [ 0.318337][ T1] brd: module loaded [ 0.330293][ T1] loop: module loaded [ 0.332521][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information. [ 0.332553][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld . All Rights Reserved. [ 0.333230][ T1] MACsec IEEE 802.1AE [ 0.333839][ T1] tun: Universal TUN/TAP device driver, 1.6 [ 0.333923][ T1] CAN device driver interface [ 0.333931][ T1] PPP generic driver version 2.4.2 [ 0.334023][ T1] PPP BSD Compression module registered [ 0.334034][ T1] PPP Deflate Compression module registered [ 0.334069][ T1] PPP MPPE Compression module registered [ 0.334080][ T1] NET: Registered PF_PPPOX protocol family [ 0.334088][ T1] PPTP driver version 0.8.5 [ 0.334429][ T1] usbcore: registered new interface driver rtl8150 [ 0.334473][ T1] usbcore: registered new interface driver r8152 [ 0.334520][ T1] usbcore: registered new interface driver asix [ 0.334559][ T1] usbcore: registered new interface driver ax88179_178a [ 0.334600][ T1] usbcore: registered new interface driver cdc_ether [ 0.334636][ T1] usbcore: registered new interface driver cdc_eem [ 0.334684][ T1] usbcore: registered new interface driver cdc_ncm [ 0.334725][ T1] usbcore: registered new interface driver aqc111 [ 0.335615][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 0.335629][ T1] ehci-pci: EHCI PCI platform driver [ 0.335673][ T1] ehci-platform: EHCI generic platform driver [ 0.336322][ T1] usbcore: registered new interface driver cdc_acm [ 0.336332][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters [ 0.336661][ T1] usbcore: registered new interface driver uas [ 0.336726][ T1] usbcore: registered new interface driver usb-storage [ 0.337065][ T1] usbcore: registered new interface driver xpad [ 0.337292][ T1] usbcore: registered new interface driver uvcvideo [ 0.337302][ T1] gspca_main: v2.14.0 registered [ 0.337755][ T1] device-mapper: uevent: version 1.0.3 [ 0.337974][ T1] device-mapper: ioctl: 4.45.0-ioctl (2021-03-22) initialised: dm-devel@redhat.com [ 0.338455][ T1] Bluetooth: HCI UART driver ver 2.3 [ 0.338472][ T1] Bluetooth: HCI UART protocol H4 registered [ 0.338503][ T1] Bluetooth: HCI UART protocol LL registered [ 0.338596][ T1] Bluetooth: HCI UART protocol Broadcom registered [ 0.338625][ T1] Bluetooth: HCI UART protocol QCA registered [ 0.339025][ T1] failed to register cpuidle driver [ 0.339124][ T1] sdhci: Secure Digital Host Controller Interface driver [ 0.339133][ T1] sdhci: Copyright(c) Pierre Ossman [ 0.339140][ T1] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.339457][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.339528][ T1] hid: raw HID events driver (C) Jiri Kosina [ 0.340798][ T1] usbcore: registered new interface driver usbhid [ 0.340811][ T1] usbhid: USB HID core driver [ 0.341108][ T1] ashmem: initialized [ 0.341554][ T1] gnss: GNSS driver registered with major 509 [ 0.342208][ T1] usbcore: registered new interface driver snd-usb-audio [ 0.342689][ T1] GACT probability NOT on [ 0.342714][ T1] Mirror/redirect action on [ 0.342741][ T1] netem: version 1.3 [ 0.342836][ T1] u32 classifier [ 0.342843][ T1] input device check on [ 0.342849][ T1] Actions configured [ 0.344410][ T1] xt_time: kernel timezone is -0000 [ 0.344561][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver [ 0.345030][ T1] gre: GRE over IPv4 demultiplexor driver [ 0.345041][ T1] ip_gre: GRE over IPv4 tunneling driver [ 0.346059][ T1] IPv4 over IPsec tunneling driver [ 0.346472][ T1] Initializing XFRM netlink socket [ 0.346513][ T1] IPsec XFRM device driver [ 0.347050][ T1] NET: Registered PF_INET6 protocol family [ 0.349106][ T1] Segment Routing with IPv6 [ 0.349153][ T1] In-situ OAM (IOAM) with IPv6 [ 0.349333][ T1] mip6: Mobile IPv6 [ 0.350047][ T1] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 0.350964][ T1] ip6_gre: GRE over IPv6 tunneling driver [ 0.351462][ T1] NET: Registered PF_PACKET protocol family [ 0.351503][ T1] NET: Registered PF_KEY protocol family [ 0.351615][ T1] can: controller area network core [ 0.351726][ T1] NET: Registered PF_CAN protocol family [ 0.351739][ T1] can: raw protocol [ 0.351757][ T1] can: broadcast manager protocol [ 0.351772][ T1] can: netlink gateway - max_hops=1 [ 0.352168][ T1] Bluetooth: RFCOMM TTY layer initialized [ 0.352197][ T1] Bluetooth: RFCOMM socket layer initialized [ 0.352249][ T1] Bluetooth: RFCOMM ver 1.11 [ 0.352266][ T1] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 0.352279][ T1] Bluetooth: HIDP socket layer initialized [ 0.352313][ T1] l2tp_core: L2TP core driver, V2.0 [ 0.352328][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0 [ 0.352336][ T1] 8021q: 802.1Q VLAN Support v1.8 [ 0.352362][ T1] tipc: Activated (version 2.0.0) [ 0.352513][ T1] NET: Registered PF_TIPC protocol family [ 0.352628][ T1] tipc: Started in single node mode [ 0.352847][ T1] NET: Registered PF_IEEE802154 protocol family [ 0.353126][ T1] NET: Registered PF_VSOCK protocol family [ 0.354108][ T1] registered taskstats version 1 [ 0.354136][ T1] Loading compiled-in X.509 certificates [ 0.357596][ T1] Loaded X.509 cert 'Build time autogenerated kernel key: 1136761ace0a26a2f73cf07655860ac1e95e7dfa' [ 0.358157][ T1] page_owner is disabled [ 0.358380][ T1] Key type ._fscrypt registered [ 0.358391][ T1] Key type .fscrypt registered [ 0.358399][ T1] Key type fscrypt-provisioning registered [ 0.361332][ T1] ALSA device list: [ 0.361370][ T1] No soundcards found. [ 0.488957][ T9] Freeing initrd memory: 18660K [ 0.489123][ T1] Warning: unable to open an initial console. [ 0.490555][ T1] Freeing unused kernel memory: 2496K [ 0.511402][ T1] Run /init as init process [ 0.515261][ T1] init: init first stage started! [ 0.516918][ T1] init: alias lines in modules.alias must have 3 entries, not 4 [ 0.517521][ T1] init: alias lines in modules.alias must have 3 entries, not 4 [ 0.519449][ T1] init: Loading module /lib/modules/zsmalloc.ko with args '' [ 0.519969][ T1] zsmalloc: module verification failed: signature and/or required key missing - tainting kernel [ 0.559871][ T1] init: Loaded kernel module /lib/modules/zsmalloc.ko [ 0.560087][ T1] init: Loading module /lib/modules/zram.ko with args '' [ 0.608164][ T1] zram: Added device: zram0 [ 0.608281][ T1] init: Loaded kernel module /lib/modules/zram.ko [ 0.608441][ T1] init: Loading module /lib/modules/soc-imx8m.ko with args '' [ 0.639674][ T1] SoC: i.MX8MQ revision 2.1 [ 0.639824][ T1] Config NOC for VPU and CPU [ 0.639920][ T1] init: Loaded kernel module /lib/modules/soc-imx8m.ko [ 0.640083][ T1] init: Loading module /lib/modules/mxc-clk.ko with args '' [ 0.911971][ T1] Bus freq driver module loaded [ 0.959762][ T1] trusty trusty: failed to get version: -1 [ 0.959783][ T1] trusty trusty: selected api version: 0 (requested 5) [ 1.039783][ T5] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 1.039818][ T40] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 1.039856][ T41] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 1.039879][ T42] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1 [ 1.071661][ T1] trusty trusty: trusty-log not supported on secure side. [ 1.119643][ T1] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1) [ 1.119659][ T1] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr [ 1.119674][ T1] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices [ 1.151750][ T1] imx-irqsteer 32e2d000.interrupt-controller: imx_irqsteer: failed to get response of echo. Use normal mode. [ 1.232064][ T1] imx8mq-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver [ 1.280046][ T1] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 43, base_baud = 1562500) is a IMX [ 3.153800][ T1] printk: console [ttymxc0] enabled [ 3.552820][ T9] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1 [ 3.664798][ T7] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO [ 3.702446][ T7] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 3.744314][ T1] i2c 0-003c: Fixing up cyclic dependency with 30b60000.mipi_csi2 [ 3.753024][ T1] pfuze100-regulator 0-0008: unrecognized pfuze chip ID! [ 3.760164][ T1] i2c 0-0050: Fixing up cyclic dependency with 38100000.usb [ 3.768642][ T1] i2c i2c-0: IMX I2C adapter registered [ 3.774841][ T1] i2c 1-003c: Fixing up cyclic dependency with 30a70000.mipi_csi1 [ 3.782857][ T1] i2c i2c-1: IMX I2C adapter registered [ 3.789465][ T1] i2c i2c-2: IMX I2C adapter registered [ 4.000761][ T1] mxs-dma 33000000.dma-apbh: initialized [ 4.063465][ T1] imx mu driver is registered. [ 4.367851][ T1] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator [ 4.377166][ T1] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator [ 4.400830][ T9] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 4.407096][ T9] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 4.411869][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: trusty driver failed to probe! nr=0xb5000000 error=-1. Use normal mode. [ 4.415577][ T9] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000000010010 [ 4.428777][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0 [ 4.438539][ T9] xhci-hcd xhci-hcd.0.auto: irq 69, io mem 0x38200000 [ 4.458957][ T9] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15 [ 4.467951][ T9] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.475895][ T9] usb usb1: Product: xHCI Host Controller [ 4.481477][ T9] usb usb1: Manufacturer: Linux 5.15.41-android13-8-00055-g4f5025129fe8-ab8949913 xhci-hcd [ 4.491312][ T9] usb usb1: SerialNumber: xhci-hcd.0.auto [ 4.497159][ T9] hub 1-0:1.0: USB hub found [ 4.501641][ T9] hub 1-0:1.0: 1 port detected [ 4.506508][ T9] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 4.512723][ T9] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 4.521097][ T9] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed [ 4.528480][ T9] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 4.537375][ T9] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.15 [ 4.546347][ T9] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.554274][ T9] usb usb2: Product: xHCI Host Controller [ 4.559855][ T9] usb usb2: Manufacturer: Linux 5.15.41-android13-8-00055-g4f5025129fe8-ab8949913 xhci-hcd [ 4.569689][ T9] usb usb2: SerialNumber: xhci-hcd.0.auto [ 4.575518][ T9] hub 2-0:1.0: USB hub found [ 4.579997][ T9] hub 2-0:1.0: 1 port detected [ 4.783893][ T1] imx-dcss 32e00000.display-controller: assigned reserved memory node secure_mm@f8000000 [ 4.793818][ T1] imx-dcss 32e00000.display-controller: dcss: failed to get response of echo. Use normal mode. [ 4.824915][ T1] cdns-mhdp-imx 32c00000.hdmi: lane-mapping 0xe4 [ 4.831250][ T1] [drm] Both HDCP 1.4 and 2.2 are enabled [ 4.839023][ T1] imx-dcss 32e00000.display-controller: bound 32c00000.hdmi (ops cdns_mhdp_imx_ops [cdns_mhdp_imx]) [ 4.851122][ T1] [drm] Initialized imx-dcss 1.0.0 20190917 for 32e00000.display-controller on minor 0 [ 5.313447][ T1] __power_supply_register: Expected proper parent device for 'battery' [ 5.323337][ T1] __power_supply_register: Expected proper parent device for 'usb' [ 5.379691][ T1] Registered IR keymap rc-empty [ 5.384764][ T1] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0 [ 5.392349][ T1] rc rc0: lirc_dev: driver gpio_ir_recv registered at minor = 0, raw IR receiver, no transmitter [ 5.403011][ T1] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input1 [ 5.505161][ T1] imx8_isi_hw: module is from the staging directory, the quality is unknown, you have been warned. [ 5.568270][ T1] init: Loaded kernel module /lib/modules/imx8-isi-hw.ko [ 5.575481][ T1] init: Loading module /lib/modules/imx8-isi-capture.ko with args '' [ 5.584165][ T1] imx8_isi_capture: module is from the staging directory, the quality is unknown, you have been warned. [ 5.634764][ T1] init: Loaded kernel module /lib/modules/imx8-isi-capture.ko [ 5.642808][ T1] init: Loading module /lib/modules/imx8-isi-mem2mem.ko with args '' [ 5.651430][ T1] imx8_isi_mem2mem: module is from the staging directory, the quality is unknown, you have been warned. [ 5.713926][ T1] init: Loaded kernel module /lib/modules/imx8-isi-mem2mem.ko [ 5.721818][ T1] init: Loading module /lib/modules/imx8-mipi-csi2-sam.ko with args '' [ 5.730696][ T1] imx8_mipi_csi2_sam: module is from the staging directory, the quality is unknown, you have been warned. [ 5.794338][ T1] init: Loaded kernel module /lib/modules/imx8-mipi-csi2-sam.ko [ 5.802597][ T1] init: Loading module /lib/modules/imx8-media-dev.ko with args '' [ 5.810877][ T1] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned. [ 5.857590][ T1] init: Loaded kernel module /lib/modules/imx8-media-dev.ko [ 5.865343][ T1] init: Loading module /lib/modules/imx-sdma.ko with args '' [ 5.916495][ T166] imx-sdma 302c0000.dma-controller: firmware found. [ 5.924245][ T166] imx-sdma 302c0000.dma-controller: loaded firmware 4.6 [ 5.939002][ T5] imx-sdma 30bd0000.dma-controller: firmware found. [ 5.943135][ T9] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 44, base_baud = 5000000) is a IMX [ 6.157877][ T1] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 6.171819][ T168] cryptomgr_probe (168) used greatest stack depth: 14312 bytes left [ 6.172379][ T1] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 16.617774][ T1] init: Wait for partitions returned after 10010ms [ 16.625671][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set): partition(s) not found after polling timeout: boot_a, dtbo_a, metadata, super, vbmeta_a [ 16.643543][ T1] init: Failed to mount required partitions early ... [ 16.657407][ T1] init: InitFatalReboot: signal 6 [ 16.668071][ T1] init: #00 pc 000000000039d350 /init [ 16.673592][ T1] init: Reboot ending, jumping to kernel [ 16.679272][ T1] kvm: exiting hardware virtualization [ 16.720193][ T1] reboot: Restarting system with command 'bootloader'