xecuting flash operation 'Program' (Program file into flash: Debug\VoiceAsst.axf) - Fri Aug 12 14:28:22 CDT 2022 Checking MCU info... Scanning for targets... Executing flash action... MCUXpresso IDE RedlinkMulti Driver v11.6 (Jul 12 2022 16:58:24 - crt_emu_cm_redlink.exe build 4) ( 0) Reading remote configuration Wc(03). No cache support. Found chip XML file in C:/GitHub_SmartRV_Panel_VA_Hardware/eng.winegard.smartpanel/Workspace_1170/VoiceAsst/Debug\MIMXRT1176xxxxx.xml ( 5) Remote configuration complete Reconnected to existing LinkServer process. Connecting to probe 1 core 0 (using server started externally) reports: 'Ee(42). Could not connect to core.' Retrying... Reconnected to existing LinkServer process. Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core. ============= SCRIPT: RT1170_connect_M7_wake_M4.scp ============= RT1170 Connect M7 and Wake M4 Script DpID = 6BA02477 Error: No power acknowledge on DAP bus Setting M4 spin code Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Setting M4 clock Error: Wire Ack Fault - target connected? Resetting M4 core Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? View cores on the DAP AP DpID = 6BA02477 Error: Wire Ack Fault - target connected? Error: Wire Ack Fault - target connected? ============= END SCRIPT ======================================== Failed on connect: Ee(42). Could not connect to core. No connection to chip's debug port (100) Target Connection Failed Unable to perform operation! Command failed with exit code 1