c2b@c2b-ubuntu01:~/Downloads/imx/imx8qxpc0mek_wayland$ bitbake imx-image-multimedia NOTE: Your conf/bblayers.conf has been automatically updated. Loading cache: 100% |###################################################################################################| Time: 0:00:00 Loaded 4951 entries from dependency cache. NOTE: Resolving any missing task queue dependencies NOTE: Multiple providers are available for runtime linux-firmware-bcm4359-pcie (firmware-nxp-wifi, linux-firmware) Consider defining a PREFERRED_RPROVIDER entry to match linux-firmware-bcm4359-pcie Build Configuration: BB_VERSION = "1.50.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-18.04" TARGET_SYS = "aarch64-poky-linux" MACHINE = "imx8qxpc0mek" DISTRO = "fsl-imx-wayland" DISTRO_VERSION = "5.10-hardknott" TUNE_FEATURES = "aarch64 armv8a crc cortexa35 crypto" TARGET_FPU = "" meta meta-poky = "HEAD:269265c00091fa65f93de6cad32bf24f1e7f72a3" meta-oe meta-multimedia meta-python = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a" meta-freescale = "HEAD:469d6c958c76ea235b3d3c1527e797ce3a7392e3" meta-freescale-3rdparty = "HEAD:f8150f3b37cb83cba1f9e2378e57bb63e02d4610" meta-freescale-distro = "HEAD:e6daa26ba1f748326546063d63a085ae671827d9" meta-bsp meta-sdk meta-ml meta-v2x = "HEAD:d6680fd8e3f1dee9556e5bc31ff49e6eecfb0937" meta-nxp-demo-experience = "HEAD:9dcc11ea9f525cffedbb28895e0abb443e56c3e0" meta-chromium = "HEAD:8be1d3a0ba0cf32e61144900597207af5698c10d" meta-clang = "HEAD:b0d805060791006d651efd3d7ae3dd5add8f70fe" meta-gnome meta-networking meta-filesystems = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a" meta-qt5 = "HEAD:43f8f539d40070a70fe89136db89bf5bb1dfe7ed" meta-python2 = "HEAD:8db9e4f6ceae33d7a4f55453d31e69f9858af4eb" meta-virtualization = "HEAD:7f719ef40896b6c78893add8485fda995b00d51d" Initialising tasks: 100% |##############################################################################################| Time: 0:00:03 Sstate summary: Wanted 11 Local 0 Network 0 Missed 11 Current 3473 (0% match, 99% complete) NOTE: Executing Tasks ERROR: tinycompress-1.1.6-r0 do_patch: Command Error: 'quilt --quiltrc /home/c2b/Downloads/imx/imx8qxpc0mek_wayland/tmp/work/cortexa35-poky-linux/tinycompress/1.1.6-r0/recipe-sysroot-native/etc/quiltrc push' exited with 0 Output: stdout: Applying patch 0001-tinycompress-Add-id3-decoding.patch patching file include/tinycompress/id3_tag_decode.h can't find file to patch at input line 224 Perhaps you used the wrong -p or --strip option? The text leading up to this was: -------------------------- |diff --git a/src/utils/Makefile.am b/src/utils/Makefile.am |index 1b996d4..e813689 100644 |--- a/src/utils/Makefile.am |+++ b/src/utils/Makefile.am -------------------------- No file to patch. Skipping patch. 1 out of 1 hunk ignored can't find file to patch at input line 236 Perhaps you used the wrong -p or --strip option? The text leading up to this was: -------------------------- |diff --git a/src/utils/cplay.c b/src/utils/cplay.c |index 87863a3..2a52b52 100644 |--- a/src/utils/cplay.c |+++ b/src/utils/cplay.c -------------------------- No file to patch. Skipping patch. 3 out of 3 hunks ignored patching file src/utils/id3_tag_decode.c Patch 0001-tinycompress-Add-id3-decoding.patch does not apply (enforce with -f) stderr: ERROR: Logfile of failure stored in: /home/c2b/Downloads/imx/imx8qxpc0mek_wayland/tmp/work/cortexa35-poky-linux/tinycompress/1.1.6-r0/temp/log.do_patch.4760 ERROR: Task (/home/c2b/Downloads/imx/sources/meta-imx/meta-sdk/recipes-multimedia/tinycompress/tinycompress_1.1.6.bb:do_patch) failed with exit code '1' NOTE: Tasks Summary: Attempted 4551 tasks of which 4550 didn't need to be rerun and 1 failed. Summary: 1 task failed: /home/c2b/Downloads/imx/sources/meta-imx/meta-sdk/recipes-multimedia/tinycompress/tinycompress_1.1.6.bb:do_patch Summary: There was 1 ERROR message shown, returning a non-zero exit code. c2b@c2b-ubuntu01:~/Downloads/imx/imx8qxpc0mek_wayland$