U-Boot 2015.04 (Sep 26 2021 - 16:22:46) CPU: Freescale i.MX6UL rev1.2 at 396 MHz CPU: Temperature 41 C Reset cause: POR Board: EPC-M6G1C I2C: ready DRAM: 128 MiB NAND: 128 MiB MMC: FSL_SDHC: 0 In: serial Out: serial Err: serial switch to partitions #0, OK mmc0 is current device Net: Phy 1 not found FEC0 Normal Boot Hit any key to stop autoboot: 0 reading dh180_a6g2c-wifi-bt-128m.dtb 35251 bytes read in 20 ms (1.7 MiB/s) reading zImage 6162784 bytes read in 285 ms (20.6 MiB/s) reading initramfs.uboot 19635758 bytes read in 869 ms (21.5 MiB/s) Kernel image @ 0x80800000 [ 0x000000 - 0x5dea38 ] ## Loading init Ramdisk from Legacy Image at 83800000 ... Image Name: Image Type: ARM Linux RAMDisk Image (uncompressed) Data Size: 19635694 Bytes = 18.7 MiB Load Address: 00000000 Entry Point: 00000000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83000000 Booting using the fdt blob at 0x83000000 Authenticate image from DDR location 0x80800000... Secure boot enabled HAB Configuration: 0xcc, HAB State: 0x99 No HAB Events Found! Using Device Tree in place at 83000000, end 8300b9b2 Starting kernel ... Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Linux version 4.1.15-starcharge-002 (chenyang@ubuntu) (gcc version 5.3.1 20160412 (Linaro GCC 5.3-2016.05) ) #33 SMP PREEMPT Mon Sep 27 14:05:39 CST 2021 CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: ZLG EPC-A6G2C Board debug: ignoring loglevel setting. bootconsole [earlycon0] enabled Reserved memory: created CMA memory pool at 0x86000000, size 32 MiB Reserved memory: initialized node linux,cma, compatible id shared-dma-pool Memory policy: Data cache writealloc On node 0 totalpages: 32768 free_area_init_node: node 0, pgdat 80ab11c0, node_mem_map 85ee7000 Normal zone: 256 pages used for memmap Normal zone: 0 pages reserved Normal zone: 32768 pages, LIFO batch:7 PERCPU: Embedded 12 pages/cpu @85ec3000 s17152 r8192 d23808 u49152 pcpu-alloc: s17152 r8192 d23808 u49152 alloc=12*4096 pcpu-alloc: [0] 0 Built 1 zonelists in Zone order, mobility grouping off. Total pages: 32512 Kernel command line: console=ttymxc0,115200 root=/dev/ram0 ro initcall_debug=1 ignore_loglevel earlyprintk=ttymxc0 PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 66348K/131072K available (7562K kernel code, 296K rwdata, 2380K rodata, 680K init, 431K bss, 31956K reserved, 32768K cma-reserved, 0K highmem) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0x88800000 - 0xff000000 (1896 MB) lowmem : 0x80000000 - 0x88000000 ( 128 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .text : 0x80008000 - 0x809bde64 (9944 kB) .init : 0x809be000 - 0x80a68000 ( 680 kB) .data : 0x80a68000 - 0x80ab23a0 ( 297 kB) .bss : 0x80ab5000 - 0x80b20f50 ( 432 kB) SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptible hierarchical RCU implementation. Additional per-CPU info printed with stalls. RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1. RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 NR_IRQS:16 nr_irqs:16 16 mxc_clocksource_init 24000000 mxsfb 21c8000.lcdif: failed to find mxc display driver Console: switching to colour frame buffer device 100x37 mxsfb 21c8000.lcdif: initialized initcall mxsfb_driver_init+0x0/0x10 returned 0 after 84979 usecs calling pxp_driver_init+0x0/0x10 @ 1 initcall pxp_driver_init+0x0/0x10 returned 0 after 5576 usecs calling sdma_driver_init+0x0/0x10 @ 1 imx-sdma 20ec000.sdma: no event needs to be remapped imx-sdma 20ec000.sdma: loaded firmware 3.3 imx-sdma 20ec000.sdma: initialized initcall sdma_driver_init+0x0/0x10 returned 0 after 21431 usecs calling pty_init+0x0/0x248 @ 1 initcall pty_init+0x0/0x248 returned 0 after 447 usecs calling sysrq_init+0x0/0xa0 @ 1 initcall sysrq_init+0x0/0xa0 returned 0 after 35 usecs calling imx_serial_init+0x0/0x50 @ 1 2018000.serial: ttymxc6 at MMIO 0x2018000 (irq = 21, base_baud = 5000000) is a IMX 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 22, base_baud = 5000000) is a IMX console [ttymxc0] enabled bootconsole [earlycon0] disabled 2024000.serial: ttymxc7 at MMIO 0x2024000 (irq = 23, base_baud = 5000000) is a IMX 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 236, base_baud = 5000000) is a IMX 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 237, base_baud = 5000000) is a IMX 21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 238, base_baud = 5000000) is a IMX ============RS485 register success by wujj at 20170504============== initcall imx_serial_init+0x0/0x50 returned 0 after 73053 usecs calling lpuart_serial_init+0x0/0x4c @ 1 initcall lpuart_serial_init+0x0/0x4c returned 0 after 700 usecs calling fsl_otp_driver_init+0x0/0x10 @ 1 initcall fsl_otp_driver_init+0x0/0x10 returned 0 after 2832 usecs calling hwrng_modinit+0x0/0xc @ 1 initcall hwrng_modinit+0x0/0xc returned 0 after 468 usecs calling drm_core_init+0x0/0x110 @ 1 [drm] Initialized drm 1.1.0 20060810 initcall drm_core_init+0x0/0x110 returned 0 after 3391 usecs calling vivante_init+0x0/0x70 @ 1 [drm] Initialized vivante 1.0.0 20120216 on minor 0 initcall vivante_init+0x0/0x70 returned 0 after 5799 usecs calling cn_proc_init+0x0/0x3c @ 1 initcall cn_proc_init+0x0/0x3c returned 0 after 11 usecs calling topology_sysfs_init+0x0/0x80 @ 1 initcall topology_sysfs_init+0x0/0x80 returned 0 after 110 usecs calling cacheinfo_sysfs_init+0x0/0x94 @ 1 initcall cacheinfo_sysfs_init+0x0/0x94 returned -2 after 3 usecs calling brd_init+0x0/0x164 @ 1 brd: module loaded initcall brd_init+0x0/0x164 returned 0 after 26766 usecs calling loop_init+0x0/0x124 @ 1 loop: module loaded initcall loop_init+0x0/0x124 returned 0 after 14561 usecs calling init_sd+0x0/0x170 @ 1 initcall init_sd+0x0/0x170 returned 0 after 272 usecs calling init_mtd+0x0/0xe0 @ 1 initcall init_mtd+0x0/0xe0 returned 0 after 446 usecs calling ofpart_parser_init+0x0/0x24 @ 1 initcall ofpart_parser_init+0x0/0x24 returned 0 after 3 usecs calling cmdline_parser_init+0x0/0x2c @ 1 initcall cmdline_parser_init+0x0/0x2c returned 0 after 1 usecs calling init_mtdblock+0x0/0xc @ 1 initcall init_mtdblock+0x0/0xc returned 0 after 8 usecs calling fsl_qspi_driver_init+0x0/0x10 @ 1 initcall fsl_qspi_driver_init+0x0/0x10 returned 0 after 1006 usecs calling cfi_probe_init+0x0/0x18 @ 1 initcall cfi_probe_init+0x0/0x18 returned 0 after 2 usecs calling jedec_probe_init+0x0/0x18 @ 1 initcall jedec_probe_init+0x0/0x18 returned 0 after 1 usecs calling of_flash_driver_init+0x0/0x10 @ 1 initcall of_flash_driver_init+0x0/0x10 returned 0 after 842 usecs calling dataflash_driver_init+0x0/0xc @ 1 initcall dataflash_driver_init+0x0/0xc returned 0 after 103 usecs calling m25p80_driver_init+0x0/0xc @ 1 initcall m25p80_driver_init+0x0/0xc returned 0 after 112 usecs calling sst25l_driver_init+0x0/0xc @ 1 initcall sst25l_driver_init+0x0/0xc returned 0 after 91 usecs calling nand_base_init+0x0/0x20 @ 1 initcall nand_base_init+0x0/0x20 returned 0 after 7 usecs calling mxcnd_driver_init+0x0/0x10 @ 1 initcall mxcnd_driver_init+0x0/0x10 returned 0 after 1030 usecs calling gpmi_nand_driver_init+0x0/0x10 @ 1 nand: device found, Manufacturer ID: 0x01, Chip ID: 0xf1 nand: AMD/Spansion S34ML01G2 nand: 128 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 gpmi-nand 1806000.gpmi-nand: mode:4 ,failed in set feature. Bad block table found at page 65472, version 0x01 Bad block table found at page 65408, version 0x01 6 ofpart partitions found on MTD device gpmi-nand Creating 6 MTD partitions on "gpmi-nand": 0x000000000000-0x000000300000 : "u-boot" 0x000000300000-0x000000400000 : "dtb" 0x000000400000-0x000000c00000 : "kernel-0" 0x000000c00000-0x000001000000 : "logo" 0x000001000000-0x000003000000 : "rootfs" 0x000003000000-0x000008000000 : "ubi" gpmi-nand 1806000.gpmi-nand: driver registered. initcall gpmi_nand_driver_init+0x0/0x10 returned 0 after 89237 usecs calling spidev_init+0x0/0xbc @ 1 initcall spidev_init+0x0/0xbc returned 0 after 167 usecs calling spi_gpio_driver_init+0x0/0x10 @ 1 initcall spi_gpio_driver_init+0x0/0x10 returned 0 after 458 usecs calling spi_imx_driver_init+0x0/0x10 @ 1 spi_imx 2008000.ecspi: probed initcall spi_imx_driver_init+0x0/0x10 returned 0 after 6585 usecs calling net_olddevs_init+0x0/0x74 @ 1 initcall net_olddevs_init+0x0/0x74 returned 0 after 27 usecs calling phy_module_init+0x0/0x10 @ 1 initcall phy_module_init+0x0/0x10 returned 0 after 1101 usecs calling can_dev_init+0x0/0x2c @ 1 CAN device driver interface initcall can_dev_init+0x0/0x2c returned 0 after 2494 usecs calling flexcan_driver_init+0x0/0x10 @ 1 2090000.can supply xceiver not found, using dummy regulator flexcan 2090000.can: device registered (reg_base=88a20000, irq=32) 2094000.can supply xceiver not found, using dummy regulator flexcan 2094000.can: device registered (reg_base=88a28000, irq=33) initcall flexcan_driver_init+0x0/0x10 returned 0 after 27782 usecs calling fec_driver_init+0x0/0x10 @ 1 2188000.ethernet supply phy not found, using dummy regulator pps pps0: new PPS source ptp0 libphy: fec_enet_mii_bus: probed fec 2188000.ethernet eth0: registered PHC device 0 initcall fec_driver_init+0x0/0x10 returned 0 after 30973 usecs calling qca_spi_driver_init+0x0/0xc @ 1 initcall qca_spi_driver_init+0x0/0xc returned 0 after 125 usecs calling ehci_hcd_init+0x0/0x70 @ 1 ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver initcall ehci_hcd_init+0x0/0x70 returned 0 after 5132 usecs calling ehci_mxc_init+0x0/0x54 @ 1 ehci-mxc: Freescale On-Chip EHCI Host driver initcall ehci_mxc_init+0x0/0x54 returned 0 after 4337 usecs calling usb_storage_driver_init+0x0/0x18 @ 1 usbcore: registered new interface driver usb-storage initcall usb_storage_driver_init+0x0/0x18 returned 0 after 4842 usecs calling ehset_driver_init+0x0/0x18 @ 1 usbcore: registered new interface driver usb_ehset_test initcall ehset_driver_init+0x0/0x18 returned 0 after 5063 usecs calling ci_hdrc_platform_register+0x0/0x1c @ 1 initcall ci_hdrc_platform_register+0x0/0x1c returned 0 after 278 usecs calling ci_hdrc_usb2_driver_init+0x0/0x10 @ 1 initcall ci_hdrc_usb2_driver_init+0x0/0x10 returned 0 after 561 usecs calling ci_hdrc_msm_driver_init+0x0/0x10 @ 1 initcall ci_hdrc_msm_driver_init+0x0/0x10 returned 0 after 432 usecs calling ci_hdrc_zevio_driver_init+0x0/0x10 @ 1 initcall ci_hdrc_zevio_driver_init+0x0/0x10 returned 0 after 414 usecs calling usbmisc_imx_driver_init+0x0/0x10 @ 1 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator initcall usbmisc_imx_driver_init+0x0/0x10 returned 0 after 7934 usecs calling ci_hdrc_imx_driver_init+0x0/0x10 @ 1 2184000.usb supply vbus not found, using dummy regulator ci_hdrc ci_hdrc.0: EHCI Host Controller ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected 2184200.usb supply vbus not found, using dummy regulator ci_hdrc ci_hdrc.1: EHCI Host Controller ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2 ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected initcall ci_hdrc_imx_driver_init+0x0/0x10 returned 0 after 97553 usecs calling gadget_cfs_init+0x0/0x20 @ 1 initcall gadget_cfs_init+0x0/0x20 returned 0 after 147 usecs calling mass_storagemod_init+0x0/0xc @ 1 initcall mass_storagemod_init+0x0/0xc returned 0 after 2 usecs calling msg_init+0x0/0xc @ 1 Mass Storage Function, version: 2009/09/11 LUN: removable file: (no medium) no file given for LUN0 g_mass_storage ci_hdrc.0: failed to start g_mass_storage: -22 initcall msg_init+0x0/0xc returned -22 after 14470 usecs calling mousedev_init+0x0/0x60 @ 1 mousedev: PS/2 mouse device common for all mice initcall mousedev_init+0x0/0x60 returned 0 after 4888 usecs calling evdev_init+0x0/0xc @ 1 initcall evdev_init+0x0/0xc returned 0 after 2 usecs calling atkbd_init+0x0/0x8 @ 1 initcall atkbd_init+0x0/0x8 returned -19 after 0 usecs calling imx_keypad_driver_init+0x0/0x10 @ 1 initcall imx_keypad_driver_init+0x0/0x10 returned 0 after 594 usecs calling imx_snvs_pwrkey_driver_init+0x0/0x10 @ 1 input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0 initcall imx_snvs_pwrkey_driver_init+0x0/0x10 returned 0 after 14033 usecs calling imx6ul_tsc_driver_init+0x0/0x10 @ 1 input: iMX6UL TouchScreen Controller as /devices/virtual/input/input1 initcall imx6ul_tsc_driver_init+0x0/0x10 returned 0 after 9393 usecs calling pcf85063_driver_init+0x0/0x10 @ 1 initcall pcf85063_driver_init+0x0/0x10 returned 0 after 110 usecs calling snvs_rtc_driver_init+0x0/0x10 @ 1 snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0 initcall snvs_rtc_driver_init+0x0/0x10 returned 0 after 9131 usecs calling i2c_dev_init+0x0/0xe0 @ 1 i2c /dev entries driver initcall i2c_dev_init+0x0/0xe0 returned 0 after 2241 usecs calling coda_driver_init+0x0/0x10 @ 1 initcall coda_driver_init+0x0/0x10 returned 0 after 938 usecs calling soc_camera_pdrv_init+0x0/0x10 @ 1 initcall soc_camera_pdrv_init+0x0/0x10 returned 0 after 247 usecs calling soc_mbus_init+0x0/0x8 @ 1 initcall soc_mbus_init+0x0/0x8 returned 0 after 1 usecs calling pxp_driver_init+0x0/0x10 @ 1 pxp-v4l2 pxp_v4l2: initialized initcall pxp_driver_init+0x0/0x10 returned 0 after 3957 usecs calling syscon_poweroff_register+0x0/0x10 @ 1 initcall syscon_poweroff_register+0x0/0x10 returned 0 after 658 usecs calling mma8451_init+0x0/0x30 @ 1 initcall mma8451_init+0x0/0x30 returned 0 after 109 usecs calling imx_thermal_init+0x0/0x10 @ 1 initcall imx_thermal_init+0x0/0x10 returned 0 after 1206 usecs calling hci_uart_init+0x0/0xe4 @ 1 Bluetooth: HCI UART driver ver 2.3 Bluetooth: HCI UART protocol H4 registered Bluetooth: HCI UART protocol BCSP registered Bluetooth: HCI UART protocol ATH3K registered initcall hci_uart_init+0x0/0xe4 returned 0 after 14856 usecs calling bcm203x_driver_init+0x0/0x18 @ 1 usbcore: registered new interface driver bcm203x initcall bcm203x_driver_init+0x0/0x18 returned 0 after 4573 usecs calling btusb_driver_init+0x0/0x18 @ 1 usbcore: registered new interface driver btusb initcall btusb_driver_init+0x0/0x18 returned 0 after 4326 usecs calling ath3k_driver_init+0x0/0x18 @ 1 usbcore: registered new interface driver ath3k initcall ath3k_driver_init+0x0/0x18 returned 0 after 4351 usecs calling cpufreq_stats_init+0x0/0xdc @ 1 initcall cpufreq_stats_init+0x0/0xdc returned 0 after 8 usecs calling cpufreq_gov_powersave_init+0x0/0xc @ 1 initcall cpufreq_gov_powersave_init+0x0/0xc returned 0 after 4 usecs calling cpufreq_gov_userspace_init+0x0/0xc @ 1 initcall cpufreq_gov_userspace_init+0x0/0xc returned 0 after 2 usecs calling cpufreq_gov_dbs_init+0x0/0xc @ 1 initcall cpufreq_gov_dbs_init+0x0/0xc returned 0 after 3 usecs calling cpufreq_interactive_init+0x0/0x15c @ 1 initcall cpufreq_interactive_init+0x0/0x15c returned 0 after 273 usecs calling imx6q_cpufreq_platdrv_init+0x0/0x10 @ 1 initcall imx6q_cpufreq_platdrv_init+0x0/0x10 returned 0 after 322 usecs calling mmc_blk_init+0x0/0x98 @ 1 initcall mmc_blk_init+0x0/0x98 returned 0 after 101 usecs calling sdhci_drv_init+0x0/0x24 @ 1 sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman initcall sdhci_drv_init+0x0/0x24 returned 0 after 7779 usecs calling sdhci_pltfm_drv_init+0x0/0x18 @ 1 sdhci-pltfm: SDHCI platform and OF driver helper initcall sdhci_pltfm_drv_init+0x0/0x18 returned 0 after 4308 usecs calling sdhci_esdhc_imx_driver_init+0x0/0x10 @ 1 /soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO sdhci-esdhc-imx 2190000.usdhc: Got WP GPIO sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA /soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified sdhci-esdhc-imx 2194000.usdhc: assigned as wifi host sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found mmc0: new high speed SDHC card at address aaaa mmcblk0: mmc0:aaaa SA08G 7.40 GiB mmcblk0: p1 mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA initcall sdhci_esdhc_imx_driver_init+0x0/0x10 returned 0 after 174372 usecs calling sim_drv_init+0x0/0x10 @ 1 initcall sim_drv_init+0x0/0x10 returned 0 after 3049 usecs calling vdoa_init+0x0/0x30 @ 1 initcall vdoa_init+0x0/0x30 returned 0 after 651 usecs calling gpu_init+0x0/0x134 @ 1 initcall gpu_init+0x0/0x134 returned 0 after 918 usecs calling gpio_led_driver_init+0x0/0x10 @ 1 initcall gpio_led_driver_init+0x0/0x10 returned 0 after 1813 usecs calling led_pwm_driver_init+0x0/0x10 @ 1 initcall led_pwm_driver_init+0x0/0x10 returned 0 after 1305 usecs calling timer_trig_init+0x0/0xc @ 1 initcall timer_trig_init+0x0/0xc returned 0 after 9 usecs calling oneshot_trig_init+0x0/0xc @ 1 initcall oneshot_trig_init+0x0/0xc returned 0 after 5 usecs calling heartbeat_trig_init+0x0/0x40 @ 1 initcall heartbeat_trig_init+0x0/0x40 returned 0 after 64 usecs calling bl_trig_init+0x0/0xc @ 1 initcall bl_trig_init+0x0/0xc returned 0 after 5 usecs calling gpio_trig_init+0x0/0xc @ 1 initcall gpio_trig_init+0x0/0xc returned 0 after 5 usecs mmc1: queuing unknown CIS tuple 0x80 (2 bytes) calling caam_driver_init+0x0/0x10 @ 1 mmc1: queuing unknown CIS tuple 0x80 (3 bytes) caam 2140000.caam: Entropy delay = 3200 caam 2140000.caam: Instantiated RNG4 SH0 mmc1: queuing unknown CIS tuple 0x80 (3 bytes) mmc1: queuing unknown CIS tuple 0x80 (7 bytes) mmc1: queuing unknown CIS tuple 0x81 (9 bytes) caam 2140000.caam: Instantiated RNG4 SH1 caam 2140000.caam: device ID = 0x0a16030000000000 (Era -524) caam 2140000.caam: job rings = 3, qi = 0 initcall caam_driver_init+0x0/0x10 returned 0 after 85081 usecs calling jr_driver_init+0x0/0x28 @ 1 mmc1: new high speed SDIO card at address 0001 initcall jr_driver_init+0x0/0x28 returned 0 after 80442 usecs calling caam_algapi_init+0x0/0x3b4 @ 1 caam algorithms registered in /proc/crypto initcall caam_algapi_init+0x0/0x3b4 returned 0 after 17478 usecs calling caam_algapi_hash_init+0x0/0x1c4 @ 1 initcall caam_algapi_hash_init+0x0/0x1c4 returned 0 after 3591 usecs calling caam_rng_init+0x0/0x220 @ 1 caam_jr 2141000.jr0: registering rng-caam initcall caam_rng_init+0x0/0x220 returned 0 after 6305 usecs calling caam_sm_init+0x0/0x58 @ 1 initcall caam_sm_init+0x0/0x58 returned 0 after 1217 usecs calling snvs_secvio_driver_init+0x0/0x10 @ 1 snvs-secvio 20cc000.caam-snvs: can't get snvs clock snvs-secvio 20cc000.caam-snvs: violation handlers armed - trusted state initcall snvs_secvio_driver_init+0x0/0x10 returned 0 after 12084 usecs calling hid_init+0x0/0x54 @ 1 initcall hid_init+0x0/0x54 returned 0 after 225 usecs calling hid_generic_init+0x0/0x18 @ 1 initcall hid_generic_init+0x0/0x18 returned 0 after 159 usecs calling hid_init+0x0/0x5c @ 1 usbcore: registered new interface driver usbhid usbhid: USB HID core driver initcall hid_init+0x0/0x5c returned 0 after 6996 usecs calling staging_init+0x0/0x8 @ 1 initcall staging_init+0x0/0x8 returned 0 after 1 usecs calling vf610_adc_driver_init+0x0/0x10 @ 1 2198000.adc supply vref not found, using dummy regulator initcall vf610_adc_driver_init+0x0/0x10 returned 0 after 7608 usecs calling alsa_timer_init+0x0/0x1f4 @ 1 initcall alsa_timer_init+0x0/0x1f4 returned 0 after 528 usecs calling alsa_pcm_init+0x0/0x6c @ 1 initcall alsa_pcm_init+0x0/0x6c returned 0 after 25 usecs calling snd_compress_init+0x0/0x8 @ 1 initcall snd_compress_init+0x0/0x8 returned 0 after 0 usecs calling snd_soc_init+0x0/0x11c @ 1 initcall snd_soc_init+0x0/0x11c returned 0 after 1164 usecs calling fsl_mqs_driver_init+0x0/0x10 @ 1 initcall fsl_mqs_driver_init+0x0/0x10 returned 0 after 942 usecs calling fsl_asrc_driver_init+0x0/0x10 @ 1 fsl-asrc 2034000.asrc: driver registered initcall fsl_asrc_driver_init+0x0/0x10 returned 0 after 6956 usecs calling fsl_sai_driver_init+0x0/0x10 @ 1 initcall fsl_sai_driver_init+0x0/0x10 returned 0 after 1755 usecs calling imx_mqs_driver_init+0x0/0x10 @ 1 imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok imx-mqs sound-mqs: snd-soc-dummy-dai <-> 2034000.asrc mapping ok imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok initcall imx_mqs_driver_init+0x0/0x10 returned 0 after 22676 usecs calling sock_diag_init+0x0/0xc @ 1 initcall sock_diag_init+0x0/0xc returned 0 after 42 usecs calling llc_init+0x0/0x24 @ 1 initcall llc_init+0x0/0x24 returned 0 after 3 usecs calling llc2_init+0x0/0xd0 @ 1 NET: Registered protocol family 26 initcall llc2_init+0x0/0xd0 returned 0 after 3233 usecs calling snap_init+0x0/0x44 @ 1 initcall snap_init+0x0/0x44 returned 0 after 7 usecs calling nfnetlink_init+0x0/0x84 @ 1 Netfilter messages via NETLINK v0.30. initcall nfnetlink_init+0x0/0x84 returned 0 after 3412 usecs calling nf_conntrack_standalone_init+0x0/0x88 @ 1 nf_conntrack version 0.5.0 (1848 buckets, 7392 max) initcall nf_conntrack_standalone_init+0x0/0x88 returned 0 after 5462 usecs calling nf_nat_init+0x0/0xac @ 1 initcall nf_nat_init+0x0/0xac returned 0 after 29 usecs calling xt_init+0x0/0x100 @ 1 initcall xt_init+0x0/0x100 returned 0 after 7 usecs calling tcpudp_mt_init+0x0/0x10 @ 1 initcall tcpudp_mt_init+0x0/0x10 returned 0 after 6 usecs calling mark_mt_init+0x0/0x44 @ 1 initcall mark_mt_init+0x0/0x44 returned 0 after 3 usecs calling connmark_mt_init+0x0/0x44 @ 1 initcall connmark_mt_init+0x0/0x44 returned 0 after 3 usecs calling xt_nat_init+0x0/0x10 @ 1 initcall xt_nat_init+0x0/0x10 returned 0 after 3 usecs calling xt_cluster_mt_init+0x0/0xc @ 1 initcall xt_cluster_mt_init+0x0/0xc returned 0 after 1 usecs calling comment_mt_init+0x0/0xc @ 1 initcall comment_mt_init+0x0/0xc returned 0 after 2 usecs calling connbytes_mt_init+0x0/0xc @ 1 initcall connbytes_mt_init+0x0/0xc returned 0 after 1 usecs calling connlabel_mt_init+0x0/0xc @ 1 initcall connlabel_mt_init+0x0/0xc returned 0 after 1 usecs calling connlimit_mt_init+0x0/0xc4 @ 1 initcall connlimit_mt_init+0x0/0xc4 returned 0 after 84 usecs calling comp_mt_init+0x0/0x10 @ 1 initcall comp_mt_init+0x0/0x10 returned 0 after 4 usecs calling iprange_mt_init+0x0/0x10 @ 1 initcall iprange_mt_init+0x0/0x10 returned 0 after 2 usecs calling ipvs_mt_init+0x0/0xc @ 1 initcall ipvs_mt_init+0x0/0xc returned 0 after 1 usecs calling length_mt_init+0x0/0x10 @ 1 initcall length_mt_init+0x0/0x10 returned 0 after 3 usecs calling limit_mt_init+0x0/0xc @ 1 initcall limit_mt_init+0x0/0xc returned 0 after 1 usecs calling mac_mt_init+0x0/0xc @ 1 initcall mac_mt_init+0x0/0xc returned 0 after 1 usecs calling multiport_mt_init+0x0/0x10 @ 1 initcall multiport_mt_init+0x0/0x10 returned 0 after 2 usecs calling cgroup_mt_init+0x0/0xc @ 1 initcall cgroup_mt_init+0x0/0xc returned 0 after 1 usecs calling recent_mt_init+0x0/0x84 @ 1 initcall recent_mt_init+0x0/0x84 returned 0 after 37 usecs calling sctp_mt_init+0x0/0x10 @ 1 initcall sctp_mt_init+0x0/0x10 returned 0 after 2 usecs calling socket_mt_init+0x0/0x1c @ 1 initcall socket_mt_init+0x0/0x1c returned 0 after 3 usecs calling state_mt_init+0x0/0xc @ 1 initcall state_mt_init+0x0/0xc returned 0 after 1 usecs calling statistic_mt_init+0x0/0xc @ 1 initcall statistic_mt_init+0x0/0xc returned 0 after 1 usecs calling string_mt_init+0x0/0xc @ 1 initcall string_mt_init+0x0/0xc returned 0 after 1 usecs calling time_mt_init+0x0/0x90 @ 1 xt_time: kernel timezone is -0000 initcall time_mt_init+0x0/0x90 returned 0 after 3002 usecs calling ip_set_init+0x0/0xb0 @ 1 ip_set: protocol 6 initcall ip_set_init+0x0/0xb0 returned 0 after 1748 usecs calling ip_vs_init+0x0/0xf4 @ 1 IPVS: Registered protocols () IPVS: Connection hash table configured (size=4096, memory=32Kbytes) IPVS: Creating netns size=872 id=0 IPVS: ipvs loaded. initcall ip_vs_init+0x0/0xf4 returned 0 after 13959 usecs calling gre_offload_init+0x0/0x10 @ 1 initcall gre_offload_init+0x0/0x10 returned 0 after 1 usecs calling sysctl_ipv4_init+0x0/0x54 @ 1 initcall sysctl_ipv4_init+0x0/0x54 returned 0 after 285 usecs calling tunnel4_init+0x0/0x70 @ 1 initcall tunnel4_init+0x0/0x70 returned 0 after 2 usecs calling ipv4_netfilter_init+0x0/0xc @ 1 initcall ipv4_netfilter_init+0x0/0xc returned 0 after 2 usecs calling nf_conntrack_l3proto_ipv4_init+0x0/0x178 @ 1 initcall nf_conntrack_l3proto_ipv4_init+0x0/0x178 returned 0 after 315 usecs calling nf_nat_l3proto_ipv4_init+0x0/0x48 @ 1 initcall nf_nat_l3proto_ipv4_init+0x0/0x48 returned 0 after 10 usecs calling nf_defrag_init+0x0/0x10 @ 1 initcall nf_defrag_init+0x0/0x10 returned 0 after 2 usecs calling ip_tables_init+0x0/0x9c @ 1 ip_tables: (C) 2000-2006 Netfilter Core Team initcall ip_tables_init+0x0/0x9c returned 0 after 3983 usecs calling iptable_filter_init+0x0/0x5c @ 1 initcall iptable_filter_init+0x0/0x5c returned 0 after 68 usecs calling iptable_nat_init+0x0/0x4c @ 1 initcall iptable_nat_init+0x0/0x4c returned 0 after 75 usecs calling masquerade_tg_init+0x0/0x24 @ 1 initcall masquerade_tg_init+0x0/0x24 returned 0 after 12 usecs calling reject_tg_init+0x0/0xc @ 1 initcall reject_tg_init+0x0/0xc returned 0 after 1 usecs calling arp_tables_init+0x0/0x78 @ 1 arp_tables: (C) 2002 David S. Miller initcall arp_tables_init+0x0/0x78 returned 0 after 3303 usecs calling arpt_mangle_init+0x0/0xc @ 1 initcall arpt_mangle_init+0x0/0xc returned 0 after 1 usecs calling arptable_filter_init+0x0/0x60 @ 1 initcall arptable_filter_init+0x0/0x60 returned 0 after 63 usecs calling inet_diag_init+0x0/0x84 @ 1 initcall inet_diag_init+0x0/0x84 returned 0 after 7 usecs calling tcp_diag_init+0x0/0xc @ 1 initcall tcp_diag_init+0x0/0xc returned 0 after 2 usecs calling cubictcp_register+0x0/0x64 @ 1 initcall cubictcp_register+0x0/0x64 returned 0 after 6 usecs calling inet6_init+0x0/0x2d4 @ 1 NET: Registered protocol family 10 initcall inet6_init+0x0/0x2d4 returned 0 after 7043 usecs calling xfrm6_transport_init+0x0/0x10 @ 1 initcall xfrm6_transport_init+0x0/0x10 returned 0 after 3 usecs calling xfrm6_mode_tunnel_init+0x0/0x10 @ 1 initcall xfrm6_mode_tunnel_init+0x0/0x10 returned 0 after 2 usecs calling xfrm6_beet_init+0x0/0x10 @ 1 initcall xfrm6_beet_init+0x0/0x10 returned 0 after 2 usecs calling sit_init+0x0/0xc8 @ 1 sit: IPv6 over IPv4 tunneling driver initcall sit_init+0x0/0xc8 returned 0 after 4967 usecs calling packet_init+0x0/0x48 @ 1 NET: Registered protocol family 17 initcall packet_init+0x0/0x48 returned 0 after 3191 usecs calling can_init+0x0/0xfc @ 1 can: controller area network core (rev 20120528 abi 9) NET: Registered protocol family 29 initcall can_init+0x0/0xfc returned 0 after 8190 usecs calling raw_module_init+0x0/0x38 @ 1 can: raw protocol (rev 20120528) initcall raw_module_init+0x0/0x38 returned 0 after 2919 usecs calling bcm_module_init+0x0/0x68 @ 1 can: broadcast manager protocol (rev 20120528 t) initcall bcm_module_init+0x0/0x68 returned 0 after 4330 usecs calling cgw_module_init+0x0/0x104 @ 1 can: netlink gateway (rev 20130117) max_hops=1 initcall cgw_module_init+0x0/0x104 returned 0 after 4492 usecs calling rfcomm_init+0x0/0xf4 @ 1 Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 initcall rfcomm_init+0x0/0xf4 returned 0 after 10243 usecs calling bnep_init+0x0/0x90 @ 1 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: BNEP socket layer initialized initcall bnep_init+0x0/0x90 returned 0 after 11447 usecs calling hidp_init+0x0/0x20 @ 1 Bluetooth: HIDP (Human Interface Emulation) ver 1.2 Bluetooth: HIDP socket layer initialized initcall hidp_init+0x0/0x20 returned 0 after 8178 usecs calling init_rpcsec_gss+0x0/0x6c @ 1 initcall init_rpcsec_gss+0x0/0x6c returned 0 after 99 usecs calling init_dns_resolver+0x0/0x11c @ 1 Key type dns_resolver registered initcall init_dns_resolver+0x0/0x11c returned 0 after 2998 usecs calling init_machine_late+0x0/0x30 @ 1 initcall init_machine_late+0x0/0x30 returned 0 after 16552 usecs calling init_oops_id+0x0/0x40 @ 1 initcall init_oops_id+0x0/0x40 returned 0 after 37 usecs calling pm_qos_power_init+0x0/0xb0 @ 1 initcall pm_qos_power_init+0x0/0xb0 returned 0 after 1252 usecs calling pm_debugfs_init+0x0/0x38 @ 1 initcall pm_debugfs_init+0x0/0x38 returned 0 after 21 usecs calling test_suspend+0x0/0x21c @ 1 initcall test_suspend+0x0/0x21c returned 0 after 2 usecs calling printk_late_init+0x0/0x5c @ 1 initcall printk_late_init+0x0/0x5c returned 0 after 8 usecs calling tk_debug_sleep_time_init+0x0/0x50 @ 1 initcall tk_debug_sleep_time_init+0x0/0x50 returned 0 after 15 usecs calling fault_around_debugfs+0x0/0x4c @ 1 initcall fault_around_debugfs+0x0/0x4c returned 0 after 13 usecs calling max_swapfiles_check+0x0/0x8 @ 1 initcall max_swapfiles_check+0x0/0x8 returned 0 after 0 usecs calling ubifs_init+0x0/0xd0 @ 1 initcall ubifs_init+0x0/0xd0 returned 0 after 842 usecs calling init_root_keyring+0x0/0x4 @ 1 initcall init_root_keyring+0x0/0x4 returned 0 after 105 usecs calling prandom_reseed+0x0/0x4c @ 1 initcall prandom_reseed+0x0/0x4c returned 0 after 36 usecs calling fb_logo_late_init+0x0/0x18 @ 1 initcall fb_logo_late_init+0x0/0x18 returned 0 after 1 usecs calling pxp_init+0x0/0x10 @ 1 initcall pxp_init+0x0/0x10 returned 0 after 666 usecs calling deferred_probe_initcall+0x0/0x88 @ 1 initcall deferred_probe_initcall+0x0/0x88 returned 0 after 2631 usecs calling genpd_poweroff_unused+0x0/0x10 @ 1 initcall genpd_poweroff_unused+0x0/0x10 returned 0 after 2 usecs calling ubi_init+0x0/0x2bc @ 1 initcall ubi_init+0x0/0x2bc returned 0 after 489 usecs calling rtc_hctosys+0x0/0xf8 @ 1 snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1) initcall rtc_hctosys+0x0/0xf8 returned 0 after 7728 usecs calling of_fdt_raw_init+0x0/0x74 @ 1 initcall of_fdt_raw_init+0x0/0x74 returned 0 after 407 usecs calling clk_debug_init+0x0/0x138 @ 1 initcall clk_debug_init+0x0/0x138 returned 0 after 17983 usecs calling register_sk_filter_ops+0x0/0x8 @ 1 initcall register_sk_filter_ops+0x0/0x8 returned 0 after 0 usecs calling tcp_congestion_default+0x0/0xc @ 1 initcall tcp_congestion_default+0x0/0xc returned 0 after 3 usecs calling ip_auto_config+0x0/0xfe8 @ 1 initcall ip_auto_config+0x0/0xfe8 returned 0 after 26 usecs calling regulator_init_complete+0x0/0x1a8 @ 1 initcall regulator_init_complete+0x0/0x1a8 returned 0 after 7 usecs calling clk_disable_unused+0x0/0x128 @ 1 initcall clk_disable_unused+0x0/0x128 returned 0 after 272 usecs calling alsa_sound_last_init+0x0/0x70 @ 1 ALSA device list: #0: mqs-audio initcall alsa_sound_last_init+0x0/0x70 returned 0 after 3109 usecs Freeing unused kernel memory: 680K (809be000 - 80a68000) Starting logging: OK Populating /dev using udev: udevd[155]: starting version 3.1.2 random: udevd urandom read with 19 bits of entropy available FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. done Starting portmap: done Initializing random number generator... done. Starting system message bus: done Starting network... Starting dropbear sshd: OK Starting sshd: OK Starting telnetd: OK Starting vsftpd: OK