U-Boot 2009.08 (Oct 20 2011 - 13:11:26) CPU: Freescale i.MX53 family 2.1V at 800 MHz mx53 pll1: 800MHz mx53 pll2: 400MHz mx53 pll3: 432MHz mx53 pll4: 455MHz ipg clock : 66666666Hz ipg per clock : 33333333Hz uart clock : 66666666Hz cspi clock : 108000000Hz ahb clock : 133333333Hz axi_a clock : 400000000Hz axi_b clock : 200000000Hz emi_slow clock: 133333333Hz ddr clock : 400000000Hz esdhc1 clock : 80000000Hz esdhc2 clock : 80000000Hz esdhc3 clock : 80000000Hz esdhc4 clock : 80000000Hz nfc clock : 26666666Hz Board: MX53-LOCO 1.0 Rev. B Boot Reason: [POR] Boot Device: SD I2C: ready DRAM: 1 GB MMC: FSL_ESDHC: 0,FSL_ESDHC: 1 In: serial Out: serial Err: serial Serial reinitilized! Net: got MAC address from IIM: 00:04:9f:01:fa:33 FEC0 [PRIME] Hit any key to stop autoboot: 3 2 1 0 MMC read: dev # 0, block # 2048, count 8192 ... 8192 blocks read: OK ## Booting kernel from Legacy Image at 70800000 ... Image Name: Linux-2.6.35.3-01073-g813d2d6-di Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3269188 Bytes = 3.1 MB Load Address: 70008000 Entry Point: 70008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... .$NkܠmY&?蹹CѲKCunVf 橿WJK&Tl* PR)$F I?iaq*B 4)tץ?+Ck uAʶT ?V ?Ue?K,*$³ + A?#$ فʱ.k鲵4Хk?)S2䤵 A?lRTl ++٥,l+ uՏPUT Ce@.W) u@. ?V+?@HUK@S 5)[ܥӹ@'3˽+,)A?UAʴQCγ3ʽ+,) AҤ+,+qK 5e(& I轲5 ְBC?.F +T䩵ZL# Sʳ9,+Р, ? fS#??ʳ lkQ6,K?#?O& I+? q@(TC ?5 A?a q@ YHPkղzC 2(ɾR iAgUqA?n ? A?(-/ ,+Р, ?$f?J.{?JAި+iAۤ, iA?;^˲4)?I+œz ެ-Ael*P غPaq? **UTl.T??H?YK #?j * ( PCة?fkSA?#?n+SA?#?V iĠ?Aa nf+?, \+T:@.EX+ܺ%$?UIJ IQTEIHB*QTUI ҢIQTak¶n A栶l"j޵+#@2YF +*䤿&3ޡZXJ5?.T+cء ARF ´a@+Cܠ+[A` , !U족,+d@* ?ʴnbcA?-+âA?6 5 @+Cܠ sDA® Q - A@.TWO +詷kA޵6m Q kAc@+,$,BctUŽbu? +A?K$޷c@+A?+S?a( E޳4+$k[E䤣+A?hbu? +S̩?a? q@.N UA?, KʲV q@.F WuݴlJʲ,బ q@.F WA?, J˲T?? $&??A¹UI?.F䠦,"&}a?5ܥ) %Aʡ*?Y]\ T"Ucޤ "&EUXV"% Iڥ5)?+SE?+@,O *˲V˲¹MY Cq@ N I5)?I+?9Kެ-AebCq@+S @,فCة?Cq@+UA?Cة?,UkEA?k?ʲI+?9Kެ,Aa k@ .N kT䩵 ʲ#&H+?.F 3ɠ.F +T䩵 fS #? $& I+?1 Р- ?#YKL %&$lf+D.F +3ޮO Ua.U(A?U Iߠ+?4.F kT䩵$& ?\ .&V? ,+3AӶ,K?$& \ &&V?I+? ߬,e I+?).$'+? S\I+?,W/+? S]I+?,J2QYb+@. A? KS? A!a*++u?+E޲Tky9F CU@!?+kEΠF CUA!?Y,$'K@,$E .W%學ɖ?ɖ?*AHꬱ 5?*'K@,$E (UJ? ,.N5??CiA?)$ qUA?+C *TKʲ SA!?Cة?@. Ac?G A蠶.Fk? SeiA?.E\V k#Aޯ+?W k#A?k$?!?V k#A̱+?2 Ke, iA A?Kҥn+s?J@.òA++? n+s?2@.ò@+#? @UtSز n+K2(kžuSٲ.i) " !z "&) Aa?Iڤ5)?@tSAز nkC2)kžtSAز.Ձʱ)?@tSAز nkC5)kžtSٲ.Ձʹ)&(-'T 5 ˲(* KʲK?Z^+,RUe?@HnRť報Tkyconsole [ttymxc0] enabled, bootconsole disabled console [ttymxc0] enabled, bootconsole disabled mxcintuart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a Freescale i.MX mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 33) is a Freescale i.MX mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX mxcintuart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a Freescale i.MX loop: module loaded pmem_adsp: 0 init pmem_gpu: 1 init MXC MTD nand Driver 3.0 i.MX GPMI NFC vcan: Virtual CAN interface driver Freescale FlexCAN Driver FEC Ethernet Driver fec_enet_mii_bus: probed PPP generic driver version 2.4.2 PPP Deflate Compression module registered PPP BSD Compression module registered PPP MPPE Compression module registered NET: Registered protocol family 24 tun: Universal TUN/TAP device driver, 1.6 tun: (C) 1999-2004 Max Krasnyansky ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1 fsl-ehci fsl-ehci.0: irq 18, io base 0x53f80000 fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2 fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200 fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00 hub 2-0:1.0: USB hub found hub 2-0:1.0: 1 port detected usbcore: registered new interface driver cdc_acm cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. usbcore: registered new interface driver usbserial usbserial: USB Serial Driver core USB Serial support registered for GSM modem (1-port) usb 1-1: new low speed USB device using fsl-ehci and address 2 usb 1-1: device descriptor read/64, error -71 usb 1-1: device descriptor read/64, error -71 usb 1-1: new low speed USB device using fsl-ehci and address 3 usb 1-1: device descriptor read/64, error -71 usb 1-1: device descriptor read/64, error -71 usb 1-1: new low speed USB device using fsl-ehci and address 4 usb 1-1: device not accepting address 4, error -71 usb 1-1: new low speed USB device using fsl-ehci and address 5 usb 1-1: device not accepting address 5, error -71 hub 1-0:1.0: unable to enumerate USB device on port 1 usbcore: registered new interface driver option option: v0.7.2:USB Driver for GSM modems ARC USBOTG Device Controller driver (1 August 2005) Android usb driver initialize android_usb gadget: android_usb ready fsl-usb2-udc: bind to driver android_usb android gadget: register function adb android gadget: register function usb_mass_storage android gadget: register function rndis rndis_function_bind_config MAC: 00:00:00:00:00:00 android_usb gadget: using random self ethernet address android_usb gadget: using random host ethernet address usb0: MAC 66:8c:38:4d:58:22 usb0: HOST MAC de:f6:de:c9:c2:e4 android_usb gadget: usb_mass_storage, version: 2009/09/11 android_usb gadget: Number of LUNs=3 lun0: LUN: removable file: (no medium) lun1: LUN: removable file: (no medium) lun2: LUN: removable file: (no medium) mice: could not register psaux device, error: -16 mice: PS/2 mouse device common for all mice input: gpio-keys as /devices/platform/gpio-keys/input/input0 MXC keypad loaded egalax_ts 2-0004: request gpio failed:-16 egalax_ts 2-0004: egalax_ts: failed to read firmware version egalax_ts: probe of 2-0004 failed with error -5 p1003_fwv33 2-0041: couldn't read panel infomation. usb 2-1: new full speed USB device using fsl-ehci and address 2 p1003_fwv33: probe of 2-0041 failed with error -5 using rtc device, mxc_rtc, for alarms mxc_rtc mxc_rtc.0: rtc core: registered mxc_rtc as rtc0 i2c /dev entries driver IR NEC protocol handler initialized IR RC5(x) protocol handler initialized IR RC6 protocol handler initialized IR JVC protocol handler initialized IR Sony protocol handler initialized Linux video capture interface: v2.00 mxc_v4l2_output mxc_v4l2_output.0: Registered device video1 usbcore: registered new interface driver uvcvideo USB Video Class driver (v0.1.0) APM Battery Driver MXC WatchDog Driver 2.0 MXC Watchdog # 0 Timer: initial timeout 60 sec device-mapper: ioctl: 4.17.0-ioctl (2010-03-05) initialised: dm-devel@redhat.com Bluetooth: Virtual HCI driver ver 1.3 Bluetooth: HCI UART driver ver 2.2 Bluetooth: HCIATH3K protocol initialized Bluetooth: Generic Bluetooth USB driver ver 0.6 usbcore: registered new interface driver btusb VPU initialized mxc_asrc registered gpu mmu disabled mxsdhci: MXC Secure Digital Host Controller Interface driver mxsdhci: MXC SDHCI Controller Driver. mmc0: SDHCI detect irq 0 irq 1 INTERNAL DMA mxsdhci: MXC SDHCI Controller Driver. mmc1: SDHCI detect irq 203 irq 3 INTERNAL DMA usbcore: registered new interface driver usbhid usbhid: USB HID core driver logger: created 64K log 'log_main' logger: created 256K log 'log_events' logger: created 64K log 'log_radio' logger: created 64K log 'log_system' Cirrus Logic CS42888 ALSA SoC Codec Driver sgtl5000-i2c 1-000a: SGTL5000 revision 17 mxc_spdif mxc_spdif.0: MXC SPDIF Audio Transmitter No device for codec mxc spdif No device for DAI mxc spdif No device for DAI imx-ssi-1-0 No device for DAI imx-ssi-1-1 No device for DAI imx-ssi-2-0 No device for DAI imx-ssi-2-1 No device for DAI imx-spdif-dai capture=0 ext_ram=0 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=f8016000 buf->area=e0856000 size=24576 capture=1 ext_ram=0 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=cf3c8000 buf->area=fa52d000 size=24576 asoc: SGTL5000 <-> imx-ssi-2-0 mapping ok mmc0: new high speed SDHC card at address 1234 usb 2-1: device descriptor read/64, error -71 mmcblk0: mmc0:1234 SA04G 3.67 GiB mmcblk0: p1 p2 p3 < p5 p6 > p4 capture=0 ext_ram=1 UseIram=1 DMA Sound Buffers Allocated:UseIram=1 buf->addr=cf3f0000 buf->area=fa533000 size=24576 asoc: mxc spdif <-> imx-spdif-dai mapping ok ALSA device list: #0: imx-3stack (SGTL5000) #1: imx-3stack-spdif (mxc spdif) nf_conntrack version 0.5.0 (13549 buckets, 54196 max) IPv4 over IPv4 tunneling driver GRE over IPv4 tunneling driver ip_tables: (C) 2000-2006 Netfilter Core Team TCP cubic registered NET: Registered protocol family 10 IPv6 over IPv4 tunneling driver NET: Registered protocol family 17 NET: Registered protocol family 15 can: controller area network core (rev 20090105 abi 8) NET: Registered protocol family 29 can: raw protocol (rev 20090105) can: broadcast manager protocol (rev 20090105 t) Bluetooth: L2CAP ver 2.14 Bluetooth: L2CAP socket layer initialized Bluetooth: SCO (Voice Link) ver 0.6 Bluetooth: SCO socket layer initialized Bluetooth: RFCOMM TTY layer initialized Bluetooth: RFCOMM socket layer initialized Bluetooth: RFCOMM ver 1.11 Bluetooth: BNEP (Ethernet Emulation) ver 1.3 Bluetooth: BNEP filters: protocol multicast Bluetooth: HIDP (Human Interface Emulation) ver 1.2 L2TP core driver, V2.0 PPPoL2TP kernel driver, V2.0 VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2 mxc_rtc mxc_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0) EXT4-fs (mmcblk0p2): recovery complete EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) VFS: Mounted root (ext2 filesystem) on device 179:2. Freeing init memory: 196K Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance. [<8003e578>] (unwind_backtrace+0x0/0xf0) from [<8046e880>] (panic+0x6c/0xe0) [<8046e880>] (panic+0x6c/0xe0) from [<800395a0>] (init_post+0xac/0xd4) [<800395a0>] (init_post+0xac/0xd4) from [<800084a4>] (kernel_init+0x124/0x168) unwind: Unknown symbol address 800084a4 unwind: Index not found 800084a4