Tutorial 3.3 How to transfer files between Windows PC / Ubuntu and the development board

Video created by Kiddy Xu on Jun 3, 2019

    The complete tutorial / FAQs are uploaded to http://www.myirtech.com/faq.asp?selectm=class&anclassid=6&nclassid=90 

    The tutorial / FAQs are based on MYIR’s NXP i.MX6UL/6ULL series products but are also applicable to similar products from other companies. MYIR hopes these are useful to you.

    MYIR’s NXP i.MX6UL/6ULL series products

    MYS-6ULX Single Board Computer

    MYD-Y6ULX Development Board (MYC-Y6ULX CPU Module as core board)

    MYD-Y6ULX-HMI Development Board (MYC-Y6ULX CPU Module as core board)

    MYD-Y6ULX-CHMI Display Panel

     

    • How to connect Ubuntu to the Internet?

    Run Oracle VM VirtualBox (this is what I am using, you may use other VirtualBox). Open the settings in the supervisor, choose network, enable network connection, connection type: bridge network card, the name of the interface: Select by actual occurrence.

    If you want ubuntu to use fixed IP, you may set it up in “Ubuntu/etc/network/interface”.

    Reference:

    # interfaces(5) file used by ifup(8) and ifdown(8)

    auto lo

    iface lo inet loopback

    auto enp0s3

    iface enp0s3 inet static

    address 192.168.30.109

    netmask 255.255.255.0

    getway 192.168.30.1

     

    • How to transfer files between Windows PC and the development board?

    The board and PC should be connected to the same network.

    Install tftpd64.exe software on the PC.

    Current Directory, choose the path to upload files.

    Server interface, choose the IP of PC. Execute “tftp 192.168.1.153 -g -r test.sh” in Xshell when downloading files to the board. Execute “tftp 192.168.1.153 -p -r test.sh” when upload files from the board to PC.

    3-3-1 tftpd64 Server configuration

    • How to transfer files between Ubuntu and the development board?

    The board and Ubuntu should be connected to the same network.

    Execute scp file to transfer files:

    “scp -r /home/roy/rs485 root@192.168.1.223:/home/root”.

    Tips: this command means copy folder ubuntu/home/roy/rs485 to directory /home/root of board with IP 192.168.1.223.