• K32W: Timeout

    In the LPC-link2 USB connection: 1. When I entered the DK6 Flash Programmer, I found that the timeout jumped out,      how many seconds will it jump out of the DK6 Flash programmer? 2. When I d...
    Daniel Tseng
    last modified by Daniel Tseng
  • iMX8M mini + 2GB DDR4 boot problems

    Dear all, I have some booting problems on my custom board based on iMX8M mini processor. We use PMIC PCA9450. Processor code MIMX8MM5DVTLZAA DDR4 DRAM code (2GB total): 2 x MT40A512M16LY-075:E   DR...
    giacomo biancalani
    last modified by giacomo biancalani
  • IMX6  VTT Termination with Pmic100 VREFDDR pin

    Hello,   I am working on imx6Q pcb board and I would like to use 4 DDR3 chips in fly-by topology.   In the 3.7§ DDR power recommendations of the Hardware Development Guide, NXP tells about DDR_VTT. I ...
    BASTIEN Guillaume
    last modified by BASTIEN Guillaume
  • K32W test tool

    I use "Test Tool 12.9.1.0" to test Multillink. The following screen will be presented without k32w selection items and the word of option may be overwritten on WIN10. How do I choose to make K32W work properly? Ca...
    Daniel Tseng
    last modified by Daniel Tseng
  • UUU tool stuck after loading bootloader image

    Hello All,   I am new to this topic of bootloader and kernal image loading. I am trying to use uuu tool and it only executes the first command of loading the bootloader. It stucks there and could not able to pr...
    Nagarjun N
    last modified by Nagarjun N
  • RT1020 - BEE decrypt on the fly on FlexSPI secondary pinmux?

    Hi.   Does the RT1020 support BEE decrypt-on-the-fly xip for FlexSPI NOR flash routed to the secondary pinmux?   Thanks and regards, Ronnie
    rshipman
    created by rshipman
  • Output a kHz range clock through a GPIO?

    Hi I'm trying to output a 4 kHz 50% duty cycle square waveform through a GPIO. What is the simplest way of doing that?  It doesn't need to be exactly 4 kHz. I accept some tolerance around the target.&...
  • K32W CMET

    I read jn-an-1242,May I ask how to use CMET in pairs?  
    Daniel Tseng
    last modified by Daniel Tseng
  • MCUXpresso and ClangFormat

    Hello,    I am working on trying to implement ClangFormat as a formatter in my MCUXPresso IDE to help save development time.  Ideally, I will be able to set up my own formatting guidelines to match my ...
    Carson Ennis
    last modified by Carson Ennis
  • LPC804 - Problem with pin P0.8

    Greetings, I'm working on a project with LPC804 (TSSOP20) and I came across a problem I can't handle. I have a simple program for capturing falling edges on pin P0.8. Pin P0.9 is used to control the thyristor and P0.1...
    Master Boy
    last modified by Master Boy
  • NXP S12G128 Debugger problem

    Hello, I am Dinesh. Currently, I am working on the NXP S12G128 board. I have installed the Free code warrior latest version and I have installed all necessarily required drivers and I am trying to switch on the LED l...
    Dinesh kovi
    last modified by Dinesh kovi
  • Debugging using IDE failed

    Tried to debug hello world program using IDE but got this following error. connected the Link USB cable J38.   Flash Driver V.2 startup failed - rc Ef(34): Timed-out initializing flash. chip initialization failed...
    haresh eswari lankaraman
    last modified by haresh eswari lankaraman
  • Trouble password protecting NTAG I²C plus

    I am trying to write a simple URL to an NFC chip (NT3H2111W0FHKH).  This is an NTAG I²C plus 1K, NFC Forum Type 2 Tag with I²C interface optimized for entry-level NFC applications.  ...
    Tyler HARNDEN
    last modified by Tyler HARNDEN
  • Error when opening project in FreeMaster

    Hello   I was following this guide (https://www.nxp.com/docs/en/application-note/AN12709.pdf ) to set up the FRDM-TOUCH, but I can't solve the error message appearing in step 7.3.  When importing...
    Niels Steyaert
    last modified by Niels Steyaert
  • Android NFC PN7150 driver porting

    Hi,   I'm trying to follow the porting guidelines found in: https://www.nxp.com/docs/en/application-note/AN11690.pdf    However, im firstly unclear on how to carry out the processes, im assuming I sh...
    Jibran Rajpt
    last modified by Jibran Rajpt
  • IMX8M IP accelerator functions

    Hello,   I try to activate the IP accelerator functions to compute the checksum of the IP header but on the reception this field is still equal to 0. I set the register TACC to 0x8 (IPCHK field set) and I set t...
    Alexandre FROISSARD
    last modified by Alexandre FROISSARD
  • Breakpoint Stopped But no Indication in MCUXpresso11.1.1

    I have a K64 project with multi-task using FreeRTOS, I noticed that some of tasks I can make BPs and step into it for debugging and MCUXpresso works properly, but some of the tasks I can make BP and the SW execution w...
    Zhiqun Hu
    last modified by Zhiqun Hu
  • Input Capture using FTM

    Dear Sir/Madame,   We are programming a board when a MCU MK20DX256VLL10 is included and connected to a driver motor. We would like to send PWM (edge aligned PWM) in a channel to the motor and know the frequency ...
    José Manuel Valero
    last modified by José Manuel Valero
  • How can we redectect usb charger?

    We have a condition where the usb power pins makes connections without the data pins when charger D+/D– detection occurs. Thus the usb charger is detect as SCP which we're relying on to set charging current. Is ...
    Prosper Van
    last modified by Prosper Van
  • can I use PSWITCH as a normal GPIO External interrupt? (disable DCDC)

    Hello colleagues, I'm working on a sensor prototype and I use MKW35 Chip. In my hardware layout I have 2 chips connected by PSWITCH and this serve as a wake-up source for mkw35. How can I configure PSWITCH to generate...
    stefan fetita
    last modified by stefan fetita