• S32K can't wake up from VLPS occasionally

    hi,     i"m using the s32k142 with RUN mode and VLPS mode, through the GPIO interrupt to wake up the chip from VLPS mode, it's working fine in most of times,but there is a slight chance that can't...
    ww ww
    last modified by ww ww
  • H.264 Hardware Encoder support on S32V234

    Hi,   We are developing an application to capture videos and want them to encode using H.264 hardware encoder in lossless mode on S32v234. I wonder if the HW H.264 Encode support lossless mode? and where can I fi...
    Muhammad Nadeem
    last modified by Muhammad Nadeem
  • problem about MPC5746R_MCAL4_0_RTM_1_0_2 license

    I use EB tresos 24.1 and  mpc5746r_ MCAL4_ 0_ RTM_ 1_ 0_ 2 developed projects,and MPC5746R_ MCAL4_ 0_ RTM_ 1_ 0_ 2. Use the free license of NXP official website. When I configuring official routines(MPC5746R_MC...
    will peng
    last modified by will peng
  • 请问IMX8M MiNi能用mfgtools烧录吗?

    我们公司买了IMX8M MiNi 板子,但是发现在windows 10下,能发现HID设备,mfgtools却无法识别,是IMX8 不能通过mfgtools烧录?UUU太复杂了,不适合生产!
    建辉 卢
    last modified by 建辉 卢
  • JLink can not support LPC5514?

    I have a Jlink V10 and it can support LPC54618 well in a previous project. But when try to use it to debug the LPC5514 in another project, and give the tips: "The selected device LPC5514 is unknow to this version of t...
    weilin ge
    last modified by weilin ge
  • iMX8M MAC to MAC Communication

    Hi,   We are working on one project and want to do MAC to MAC communication.   Requirement: iMX8M to iMX8M communication over MAC.   We have done following connections in the schematic:   MAC1_...
    Sahil Nayak
    last modified by Sahil Nayak
  • Custom camera driver adaptation on iMX8M Mini

    Dear experts,   I'm in the process of porting a custom camera to iMX8M Mini from its original driver dedicated to Nvidia Jetson platforms. I've finished the control part via I2C bus. However, I've got following...
    Khang Le Truong
    last modified by Khang Le Truong
  • Sir when I do Pinsel for CAN 1 RX which is 0x00040000 the board resets Please help me.I have attached the code below

    #include<lpc21xx.h> char a[100]={1,3,5,7,9,11,13,15}; char b[100]={2,4,6,8,10,12,14,16}; char rxdata[8]={0,0,0,0,0,0,0,0}; char txdata[8]={0,0,0,0,0,0,0,0}; int flag=1; unsigned int l,id; unsigned int low...
    Akhilesh Vernekar
    last modified by Akhilesh Vernekar
  • EVB9S12XF512E RTI not generated

    Development board:          EVB9S12XF512E  Target Processor:           MC9S12XF512MLM Operating system:           N.A....
    Rohit Ramakrishnan
    last modified by Rohit Ramakrishnan
  • SPC5744上电后一直复位

    使用SPC5744做的新板子,上电后测量单片机电压3.3V为3.268V,内核1.25V实测1.223V,上电后单片机第31脚-RESET脚持续输出 接近0V的低电平,造成板子无法连接编程器。
    mian fang
    last modified by mian fang
  • MPC5775E/MPC5775B eQADC vector table entry clarification?

    Hello Everyone, Looking at the MPC5775E reference manual (Rev 1 May 2018) which also covers the MPC5775B, there is a features table that shows the ADC Quantity as 4 on the MPC5775E and 2 on the MPC5775B. However, the...
    iansmusical
    last modified by iansmusical
  • KW36 flexcan how to receive all CAN id

    I am using frdmkw36_driver_examples_flexcan_interrupt_transfer and I want to receive all can id. I set rxIdentifier to 0x00, input 'B', send CAN message. The KW36 can receive my message, but t...
    mo xinyu
    last modified by mo xinyu
  • Module 1: Environment Setup

    INTRODUCTION In this module of the 3-Phase PMSM Workshop, the focus is on the hardware and software setups that are going to be used throughout this workshop to implement and test a complete 3-phase Permanent Mag...
    dumitru-daniel.popa
    last modified by dumitru-daniel.popa
  • SE050C2HQ1/Z01SDZ- Termination finish

    Hello team,   We need your advice regarding the termination finish of #SE050C2HQ1/Z01SFZ.   a. In the case of 100% tin please advise:       i. What kind of tin is used, ...
    Shai Berman
    last modified by Shai Berman
  • trouble about flexray model on MPC5744

    I am trying to develop the flexray module on MPC 5744 ,but it can't go to the state called normal active. and the oscilloscope can't see anywaveform.   the bitfield called PROTSTATE in the PSR0 register...
    耀真 卢
    last modified by 耀真 卢
  • Classic - How to use dashboard (Jenkins) to build a CodeWarrior project?

    Classic - How to use dashboard (Jenkins) to build a CodeWarrior project?             Valid for all Classic IDE versions - CW for MCU V6.x, CW for PA V8.8, etc ......
    Pascal Irrle
    last modified by ebiz_ws_prod
  • S32K1XX SCLS and SDAS can use it by 2-Wire Scheme?

    Hi   When I use SCLS and SDAS separately to make IIC2 cable system, it seems not to work         When I checked the manual, I found that this is not supported, only used under the 4-wire s...
    建宽高
    last modified by 建宽高
  • How flashing works in K32L2B in production board

    Hey, I'm trying to figure out the requirements for the production board so we can flash from the factory as well as in production. We are using the same MCU as in the FRDM-K32L2B3 dev kit. Could somebody read this and...
    Eric Smith
    last modified by Eric Smith
  • S08PT60 Evaluation Kit, lookinf for example code in C/C++

    Hello team,   My customer plan to work with #MC9S08PL4 and the closed EVK available is #S08PT60-EVK. when I started to work with S08 SDK (using code warrior 11.1) I found out that all the example code...
    Shai Berman
    last modified by Shai Berman
  • imx6dq 升级android6.0后,千兆网不可用

    dear all imx6dq with ar8035,in android4.3,Gigabit Ethernet is working well ; but now we upgrade to android6.0,and kernel4.1.15; Gigabit Ethernet is not  working ,and ping  failed ,do you have idea to solv...
    卫 陈
    last modified by 卫 陈