• /dev/ttyACM* missing after reboot

    Hi I was working without any problem with a MODEM connected via /dev/ttyACM* to my IMX6ULL in aour custom board.   I executed a reboot on the processor without switch off (both MODEM and IMX6ULL)   the /d...
    fabio mario poiatti
    last modified by fabio mario poiatti
  • microSD Card not working in custom imx7d board

    Greetings! I am using micro SD Card in my custom imx7d board in accordance with the reference of the imx7d Sabre board. The issue I am facing is I am getting the initial pulse of SD card detection on SD1_CLK pin, whe...
    Vikrant A P
    last modified by Vikrant A P
  • IMX8QM DSI to LVDS bridge voltages

    Hi guys. I'm trying to implement a DSI to LVDS bridge for the iMX8QM. From searching here, the SN65DSI83 / 4 seem popular options on other iMX variants. From what I can see from the iMX8QM reference design documentati...
    Peter Bain
    last modified by Peter Bain
  • Capture image issues with IMX7D and CSI (CMOS)

    Hello community, I have several questions regarding capturing a single picture using CSI interface. I have set up parallel sensor and csi driver (mx6s_capture.c). Driver for camera was ported to use subdev and succe...
    Eddie Vazquez
    last modified by Eddie Vazquez
  • Cannot open MCUXpresso Config tools from V11.1

    I just installed MCUXpresso V11.1 I created a new workspace and created a New Project based on the MK60DN512xxx10 controller.     I then select the MCUXpresso Config Tools>>Open Peripherals and I ...
    Terry Biberdorf
    last modified by Terry Biberdorf
  • Gyroscope: FXAS2100x Breakout Board

    Hi,   The FXAS2100x, is a small, low-power, yaw, pitch, and roll angular rate gyroscope with 16 bit ADC resolution. The full-scale range is adjustable from ±250°/s to ±2000°/s. It features bo...
    Jose Alberto Reyes Morales
    last modified by Adrian Puga Candelario
  • RT1052 CSI - stuck waiting for GetFullBuffer

    We are using the CSI in our custom RT1052 board, our code is BASED on the AN12110SW, but as we don't have an LCD, our camera is monochrome, etc - it's been altered according to our hardware.      I can...
    variable_andrew
    last modified by variable_andrew
  • AndroidSDCARDMirrorCreator

    This tool is also for emmc user partition mirror. Just give this tool the emmc files. The typical use case is for emmc mass production by emmc offline programming.   Ver 0.4.0 2/14/2017 Support And...
    Biyong Sun
    last modified by Adrian Puga Candelario
  • How to configure debug target for i.MX RT that flashes the board?

    Hi All   I am making my first attempt to use MCUXpresso to debug a target but presently is fails since it doesn't seems to load any code to the board and also doesn't seem to do behave normally when connected (I...
    Mark Butcher
    last modified by Mark Butcher
  • MPC5643L PWM_ADC measurement concept

    The aim of the MPC5643L PWM triggered measurement concept is to introduce hardware  subsystem concept of autonomous triggering of ADC measurement by PWM module in desired time intervals and automatic storing of m...
    Peter Vlna
    last modified by Adrian Puga Candelario
  • UART with input data as string

    Hello, The below attachment is the code for UART with the input data as a character..But i need the input data to be a STRING...Can anyone please post the code for UART with input as a string using MK22D5.
    sarvani adabala
    last modified by Adrian Puga Candelario
  • I need to connect "AD5933 Chip" to NFC circuit by I2C connection

    Hey, I want to connect my circuit through "AD5933 Chip" to NFC by I2C connection, I looked at several products that have NFC technology, but I am not sure that those products are relevant to my project....
    Aviad Megira
    last modified by Aviad Megira
  • Exercise 2: Toggle all 4 LEDs on the K60 Tower using the PIT0

    To do:   Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt. For easy debugging, let the program run in the RAM.   * toggle period 0.5 s, * extract vector ta...
    peterurbanek
    last modified by Adrian Puga Candelario
  • Where to find latest SDMA firmware for imx6ul?

    Hi,   Looking for the latest SDMA firmware for the IMX6UL.  I have 3.3   Thanks
    Jim Brooke
    last modified by Jim Brooke
  • Patch to enable SSI_ASRC_P2P_capture function based on Kernel_3.0.35_SabreSD_Board

    Here are two patchs: Patch 1: 0001-I.MX6-SSI_ASRC_P2P_Capture-for-SabreSD-board-Kernel-.patch Patch 2: 0001-I.MX6-SSI_ASRC_P2P-Capture-for-SebreSD-board.patch Patch 1 is based on patch 2.     memory &...
    Lei Ge
    last modified by Adrian Puga Candelario
  • Frdm KE15z "0 available SWD Devices detected. Connect a device and try again"

    Hi,    I am having a problem. When trying to initiate Debug, the probe is detected: But when I pressed OK button, it cannot access to SWD link: I tried with reset button, restart my computer, bu...
    Nguyen Dao
    last modified by Nguyen Dao
  • Is there a more detailed documentation of the USB-Stack?

    Hello, I want to know how to use the USB-Stack. Is there somewhere a more detailed documentation/Application Note than the one provided with the SDK download? The provided examples work but do not explain the concept...
    Stefan Mitterhauser
    last modified by Stefan Mitterhauser
  • How to Disable RF

    Hi,  I am working on the PN7462AU Eval Kit for the Contactless(CL) card & Contact(CT) card reader with "phExCcid" example. And I need to switch OFF the RF and only need to ON the functionality for the Conta...
    Manva Trivedi
    last modified by Manva Trivedi
  • MCUXpresso IDE v11.1.0 SDK Handling Hotfix

    An issue has been identified in MCUXpresso IDE v11.1.0 with SDK 2.7 that in certain circumstances can cause the IDE to issue one or more erroneous duplicate file error popups when importing SDK examples or creati...
    LPCX presso support
    last modified by LPCX presso support
  • i.MX51 WINCE600 eCSPI Support Multiple Bursts Mode and Wait States

    In the i.MX51 default WINCE6  release, the eCSPI doesn't support multiple bursts mode and set the wait states. Attached was the document and code for how to enable the multiple bursts mode and how to set the wai...
    Justin Jiang
    last modified by Adrian Puga Candelario