Hi everybody,
I am using linux-2.6.35.3 ltib kernel for booting tx28 karo module. But we have done the pin muxing changes. Then also the kernel is not booting . Please refer the below log message.
Booting kernel from Legacy Image at 42000000 ...
Image Name: Linux-2.6.35.3-571-gcca29a0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2368916 Bytes = 2.3 MB
Load Address: 40008000
Entry Point: 40008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
It stops at this point. Can anybody tell me should i make any another changes to overcome the above problem.
Rgds,
G.Venkatesh Kumar