AnsweredAssumed Answered

ESCI_A.SR.B.RDRF flag is not set on mpc5634xm uController

Question asked by andrea mocci on Nov 2, 2011

Hi everybody.

Actual severity of this issue is more than super critical!
I am developing a diagnostic application based on eSCI transmission; an external diagnostic tool will connect to the ECU using serial communication and standard KWP2000 protocol; K-Line uses eSCI peripheral to start, stop and handle communication with the ECU; unfortunately, tracing data through Lauterbach Trace32, I have seen that when I send an SCI frame (oscilloscope confirms that it arrives correctly to RXDA pin in the uController) the ESCI_A.SR.B.RDRF flag is not set (a break point in read/write access confirms it), so it is not possible for me to catch the ISR and to do next operations.
Why? Have you got any suggestions?

 

Thank you in advance

 

Andrea

Outcomes