I have installed Eclipse CW version.
Solved! Go to Solution.
I had unzipped the file and did not unterstud what to do with its content (jar file).
Now I managed to install but I get an error:
Hello,
you need to install the latest update to the 10.1 (as this is not present in the base 10.1):
Then you find the setting in the 'Interrupts' debugger settings:
BK
I have the 10.1 version, but in the debug configuration I do not see the interrupt tag
You need at least the 1.0.1 update for the 10.1 release.
Available from
there select the 'download tab'
and download/install
MCU 10.1 Update for Windows: Adds Kinetis K50 family support, Processor Expert support for Kinetis 144, 100, and 80 LQFP packages, and Kinetis example projects.
Size (K): 275127 Format: zip Rev #: 1.0.1 Modified: 8/15/2011
Then the option should show up.
BK
I have downloaded the MCU 10.1 Update for Windws but now I cannot able to upgrade it.
How can i update with Jar file ?
Thanks
Menu Help > Install New Software.
Then press 'Add' button.
Use the 'Archive...' button to browse for the zip file you have downloaded.
BK
I had unzipped the file and did not unterstud what to do with its content (jar file).
Now I managed to install but I get an error:
I see that you have CW installed in C:\program files. If you are using Vista or Windows 7: make sure you run the update as administrator. Otherwise Windows might deny installation of files.
BK
OK, now I have installed in Administrator mode and the installation proceed.
Moreover I have a timeout error:
OK, now connection with server OK.
All installed and Interrupt tag displayed !! :smileyhappy:
Thanks for help