Hello,
I just created an executable (.elf) with CodeWarrior 2.7, and I would like to know if it works.
I try to use Lauterbach for connected Computer-Eval Board. The name of this is : "Debuger USB2 Power debug interface". I have installed it, but CodeWarrior dont detect him.
Can you help me for found out if i forgot someting.
Thank you.
Best regard.
What version of Windows are you running?
Did you install the drivers for the Lauterbach run control device?
---Tom
Thank you for your help.
I use Windows XP (SP3).
I installed the driver for Launterbach run control device. He works well with Trace32.
In CodeWarrior, have you checked all of the debugger settings panels? Specifically, there should be some remote debug settings or connection settings where you choose the run-control device/interface. Is the Lauterbach visible there?
Sorry I can't be more specific because I don't have that version of CodeWarrior.
---Tom
Sorry but i don't undersand what is for you: "the debugger settings panels" ?
In "Edit/Preference...", I don't find any information about a debugger settings panels.
After a successful compilation, a pop-up opens. In this pop-up there is a combo box with 5 choose:
I can't find Lauterbach.
Thank you for your help and good week.
You probably don't see any debugger settings panels because CodewWarrior hasn't found a debug probe yet. According to this Freescale page, Lauterbach probes are supported. The only choice that makes sense is the PPCNEXUS one. This same page also advises when using a Lauterbach: "Please read TargetingMPC55xx.pdf located in the Help\pdf folder of your CodeWarrior installation."
---Tom
Indeed, a solution is described here: TargetingMPC55xx.pdf, page 79. We must create a .cmm file to use CodeWarrior and Lauterbach together. Unfortunately I can't integrate with an existing project...
Again thank you for your help. Good day.