Hi all
I am using CW for PA 10.0.2 with the latest update installed and also have a USB TAP. What I would like to do is to use the TAP to debug an image built under a different toolchain.
I can load the code and run/debug it but I cannot get CW to perform source level debugging, it always says that the source files cannot be found. So as it stands, I can only debug in assembler but I really need to cebug in C. I have followed the instructions in the Targetting Manual but this does not seem to work.
Has anyone managed to get this working and if so can you give me some help? Or perhaphs this is not possible as the code was built using a different compiler?
Thanks
Obi
Hello
As the application has not been built within CodeWarrior the debugger has trouble to find the source files if :
A- The executable file debug info does not include full paths to the actual source code.
Depending on the =tools you are using for building you may have an option to store the full path to the
source files in the debug info.
B- The executable file has been built on another system or you do not have the ability to add full path information
to the debug information.
In this case you need to add path mapping information
This is done as follows:
CrasyCat