AnsweredAssumed Answered

Is it possible to use two IntEEPROM beans, simultaneously?

Question asked by Anders Johansson on Aug 18, 2011
Latest reply on Aug 19, 2011 by Processor Expert

HCS12XEP100, IntEEPROM bean and PE V2.99.

 

I want to use 4096 bytes of emulated EEPROM.

In addition to that I want to use more of the EEPROM

and access it with the SetByte and Get Byte functions.

 

I added two beans and set up the Start adresses and used sizes accordingly,

but PE complains about using the bean twice.

 

Is it not possible to set up more than one IntEEPROM bean?

 

If not, how do I use emulated and NOT emulated EEPROM simultaneously?

 

Thanks,

Anders J

Outcomes