Gary Johnson

CW 6.3 MCF51JM128 Debugging Memory Map "overlapping memory"

Discussion created by Gary Johnson on Aug 12, 2011
Latest reply on Aug 31, 2011 by CrasyCat

Anyone understand the error message below?

 

MCF51JM128 Debugging Memory Map


-A memory range from 0x3fe to 0x40f is of "internal" type for display purpose.


-A memory range from 0xc00000 to 0xc0000f is of "internal" type for display purpose.


-A memory range from 0xffff8000 to 0xfffffffc is of "internal" type for display purpose.  WARNING: This module is overlapping with module having Comment:"Memory Mapped Reg. Block 4".


-A memory range from 0xffff98a1 to 0xffff98b2 is of "internal" type for display purpose. WARNING: This module is overlapping with module having Comment:"Memory Mapped Reg. Block 3".


-A memory range from 0x0 to 0x1ffff is of "physical" type,therefore accessed directly in device physical memory (0x0-0xffff).


-A memory range from 0x800000 to 0x803fff is of "physical" type,therefore accessed directly in device physical memory (0x0-0xffff).

 

Thanks, gj

Outcomes