MCF52233 ADC POWER PINS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF52233 ADC POWER PINS

465 Views
DariusB
Contributor I

Hello,

 

I am using  MCF52233 MPU, but not using ADC. 

 

Can I disconnect VDDA and VSSA pins from power lines? (Possible reduce power comsumption?)

If not, other question?

Can I replace Ferrite bead and L1  (filters of ADC power)  with R0?

Labels (1)
0 Kudos
1 Reply

250 Views
scifi
Senior Contributor I

Can I disconnect VDDA and VSSA pins from power lines? (Possible reduce power comsumption?)

The datasheet says that analog supply voltage must be between 3.0V and 3.6V. So I guess it means no, you cannot disconnect analog supply. I suspect that even if you did, the ADC would still draw current from the digital supply through on-chip diodes (that are likely present.)


Can I replace Ferrite bead and L1  (filters of ADC power) with R0?

This should be safe.

0 Kudos