Hello,
I just want to know if the issue below is knowed :
I can flash a my application on my board on the mpc5534, with the USB multilink except when the aggressive_inline option is set.
(in the preprocessor tab, I've set : #pragma aggressive_inline on )
The error messages are really not explicit.
With a Lauterbach interface it is ok, with a CAN reprogrammation (through a bootloader) it is ok.
Does someone get the same issue?
Regards,
Briag, Automotive, Toulouse, France
Hello Briag,
This is really weird issue. Assume you build with CodeWarrior.
Which version of CodeWarrior are you using? (Menu Help -> About ->Installed Products)
If I understand this issue correctly:
- you are able to build the application with aggressive_inline option set (no link errors).
- then you can program generated flash image (.elf) into controller MPC5534 using Trace32.
- you are unable program the same image into controller using P&E ICD. Error during Flash programming?
Could you post an P&E Flash programming error screenshot?
Stanish