MQX Serial Driver: the ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX Serial Driver: the ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented

Jump to solution
910 Views
Icenine
Contributor I

Hello!

 

The ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented for the Kinetis platform.

 

MQX version: 3.7

0 Kudos
1 Solution
351 Views
DavidS
NXP Employee
NXP Employee

Hi Icenine,

The Kinetis SCI modules do not support anything other than 1-bit stop therefore no need to have IOCTL command.

Regards,

David

View solution in original post

0 Kudos
1 Reply
352 Views
DavidS
NXP Employee
NXP Employee

Hi Icenine,

The Kinetis SCI modules do not support anything other than 1-bit stop therefore no need to have IOCTL command.

Regards,

David

0 Kudos