Hello all,
Since I moved to Windows 7 I receive an error almost everytime I close CodeWarrior IDE v10.1. I use CodeWarrior to create bareboard projects for the HCS08QE family devices, and this is the error I get:
I've investigated a bit and it seems the error is thrown if I run or debug an application. If I open CodeWarrior and do not run or debug any project, I can close CW without any error.
Going further, when running or debugging a project, I noticed a new process called DE.exe is launched by CodeWarrior, see it selected in the following image:
That process is initialized when transferring the project to the CPU, but it is not closed when finished. So, I think the error I receive when closing CW can be caused because that process is still alive or something. As I said, if that process is not initialized I can close CW without errors.
Has anyone seen the same behavior? Is there any possible fix? It is a bit annoying receiving that error anytime I close CW...
Thanks!
Diego.
I believe that DE.exe is the CodeWarrior debugger engine being activated when you run or debug a project. That is normal behavior. You need to file an on-line service request to report this problem.
---Tom