donw

CW debugger not loading source code

Discussion created by donw on Jul 19, 2011
Latest reply on Jan 22, 2015 by Peter Gawell

I have made a new project with CodeWarrior and copied into it an existing code file, as I have done OK in the past.

(machine code only, absolute assembly)

Two problems occur, (which may be related) , when I start a Debug session:

 

1) On debug startup, a Yes/No window shows which states:

   'Enable Debugger for Target 'standard'. The debugger requires certain target settings in order to function correctly. Do you         want  CW to configure these settings automatically for target 'standard' ?

 

2) the source code does not load into the debugger....

 

Any ideas how to fix these problems?

CW v5.9.0, Debugger v6.1,  '08JM60 cpu.

Outcomes