Meir Yeru

UART Max Baud Rate MCF52259

Discussion created by Meir Yeru on Jul 18, 2011
Latest reply on Jul 20, 2011 by Mark Butcher

Hello

 

I working with MCF52259 MCU

I need to transfer string between 2 uart's - What is the MAX bauderate than the MCU capable?

What are the crystal than I need connect to MCU to get the max bauderate ?

(Can I use 48MHz and double it with the PLL and clock the uart with that clock??)

 

I want to use 921,600bps or higher

 

 

Many thanks,

 

Mayer

Outcomes