I cannot communicate with the board so I am wondering if the right USB driver got installed.
The debugger cable is simply a usb cable to a socket on the board--no bdm multilink necessary.
I let WindowsXP install the driver and it chose "Open Source BDM-JM60 (libusb-w32)".
Can anyone confirm that this is the correct driver?
I have already installed different drivers for an LL16 demo board and USB BDM MULTILINK.
THe OSBDM driver is correct.
The problem is that the TWR_S08LL64 comes pre-programmed with an app that disables the debugger in a low power mode.
Pushing a button causes the app to wake up the CPU and get a clock to the debugger. Communication can then take place.