Dear All,
I am trying to open for debug a .elf with Codewarrior for MPC55xx v2.3. I have the settings that appear on the manual Targeting MPC55xx (Preferences->Build->Never and Cache disabled).
When drag % drop the file Codewarrior says "Codewarrior cannot open this type of file".???. It is very important this for me because I use makefiles for compiling/linking and then .elf for debugging.
Am I forggeting something?
Thanks a lot and best regards,
ispd
Hello, it is bypassed by using the a .bat and running the debugger from the bat.
Putting this on a .bat file I was able to do it.
"C:\Archivos de programa\Freescale\CodeWarrior for MPC55xx V2.3\pemicro\cw_icdppcnexus.exe" App.elf LOADTORAM -RESETFILE "C:\Archivos de programa\Freescale\CodeWarrior for MPC55xx V2.3\pemicro\mpc5500_booke.mac" LOADGOTILMAIN -SOURCEPATH ".\"